7.3.1 Application Configuration
In this release, there are 4 hex files and 2 projects included
The hex files are named as follows:
- demo_app_udp_ftd_leader.hex
- demo_app_udp_ftd_router.hex
- demo_app_udp_mtd_med.hex
- demo_app_udp_mtd_sed.hex
It is recommended to first flash the demo_app_udp_ftd_leader.hex file and then flash the remaining hex files to their respective nodes.
Additionally, there are 2 projects bundled with this release:
- demo_app_udp_ftd
- demo_app_udp_mtd
Once the hex files have been flashed as per the release details, the nodes will automatically form a network and begin transmitting data.
To configure FTD as a leader
Please open the demo_app_udp_ftd.x file using MPLAB X IDE and navigate to the thread_demo.h file as directed.
Please modify the macro DEVICE_AS_LEADER to a value of 1, as demonstrated below:

Navigate to udp_demo.h as shown below.

Please access the file udp_demo.h as demonstrated below.

The project now includes a Leader functionality that offers the same features as the demo_app_udp_ftd_leader.hex.
To configure FTD as a router
Please open the demo_app_udp_ftd.x file using MPLAB X IDE and navigate to the thread_demo.h file as described previously.
Edit the macro DEVICE_AS_LEADER to 0 as shown below.
Please navigate to the file udp_demo.h and implement the modifications as indicated below.
The project now includes Router functionality that is identical to the functionality found in the demo_app_udp_ftd_router.hex file.
To configure MTD as an MED
Please open the demo_app_udp_mtd.x file using MPLAB X IDE and navigate to the thread_demo.h file as described previously.
Edit the macro DEVICE_AS_LEADER to 0 and ENABLE_SLEEP to 0 as show below.
Navigate to the file udp_demo.h and implement the modifications as indicated below.

Now the project has MED functionality having the same functionality as demo_app_udp_mtd_med.hex
To configure MTD as SED
Please open the demo_app_udp_mtd.x file using MPLAB X IDE and navigate to the thread_demo.h file as described previously.
Edit the macro DEVICE_AS_LEADER to 0 and ENABLE_SLEEP to 1 as show below.
Navigate to the file udp_demo.h and implement the modifications as indicated below.

The project now includes SED functionality that is equivalent to the functionality found in demo_app_udp_mtd_sed.hex.