4 Get Source Code from Atmel START
The example code is available through Atmel START, which is a web-based tool that enables configuration of application code through a Graphical User Interface (GUI). The code can be downloaded for both Atmel Studio 7.0 and IAR™ IDE via the Examples-link below, or the BROWSE EXAMPLES button on the Atmel START front page.
Web page: http://start.atmel.com/
Documentation: http://start.atmel.com/static/help/index.html
Examples: http://start.atmel.com/#examples
In the Examples-browser, search for: Core Independent Nightlight Using CCL on ATtiny1617 (press User Guide in Atmel START for detailed requirements for the example project).
Double-click the downloaded .atzip file and the project will be imported to Atmel Studio 7.0.
For information on how to import the project in IAR, press the Documentation-link above, select ̔Atmel Start Output in External Toolsʼ and ̔IAR Embedded Workbench®ʼ.