7.4.3.3 Function ac_chan_get_status()
Determines the output state of a comparator channel.
uint8_t ac_chan_get_status( struct ac_module *const module_inst, const enum ac_chan_channel channel)
Retrieves the last comparison value (after filtering) of a given comparator. If the comparator was not ready at the time of the check, the comparison result will be indicated as being unknown.
| Data direction | Parameter name | Description |
|---|---|---|
|
[in] |
module_inst |
Software instance for the Analog Comparator peripheral |
|
[in] |
channel |
Comparator channel to test |
Returns
Bit mask of comparator channel status flags.