7.2.3 Struct ac_events
Event flags for the Analog Comparator module. This is used to enable and disable events via ac_enable_events() and ac_disable_events().
| Type | Name | Description |
|---|---|---|
| bool | generate_event_on_state[] |
If true, an event will be generated when a comparator state changes |
| bool | generate_event_on_window[] |
If true, an event will be generated when a comparator window state changes |
| bool | on_event_sample[] |
If true, a comparator will be sampled each time an event is received |