6.1.1 Plotting Graph in Data Visualizer
The following instructions show how to plot USART data in Data
Visualizer by using the Data Stream protocol.
- Open Data Visualizer.
- Open in Data Visualizer.
- Select the Curiosity
Virtual COM port, Baud rate:
9600
and then select Connect. - Open
- In Data Stream
Control Panel, under
Configuration, browse to the
configuration file and then select Load.Note: In this case, the configuration file is
and can be found in the example source code project folder.single_measuring_VDD/single_VDD_voltage.txt
Note: For more details on the Data Stream Protocol, refer to Data Visualizer User's Guide, Data Stream Protocol section.
- Open .
- Drag the connections as shown with red arrows in the figure below to plot the graph.
To adjust the Y-axis in the graph, follow the steps below:
- Under Configuration in Graph, deselect Automatically Fit Y.
- Click somewhere inside the plot area.
- Scroll the mouse-wheel while pressing or holding the Ctrl key.
To adjust the X-axis in the graph, follow the steps below:
- Click somewhere inside the plot area.
- Scroll the mouse-wheel while pressing or holding the Shift key.
Note: For more details on , refer to the Data Visualizer User's
Guide, Graph section.