5.5.4 CMD: GET

Used to get parameters on the tool.

For lists of valid get/set parameters, see Housekeeping SET/GET Parameters.

Table 5-12. Get
FieldSizeDescription
GET (0x02)1 byteCommand ID
Version (0x00)1 byteCommand version
Get context1 byteContext of the parameter to get
Address1 byteParameter ID/start address
Bytes1 byteNumber of bytes to read

Responses:

Note: Getting multiple parameters in one set call can only be done when all fields are in the same context.