1.6 SST26 SQI Flash Driver - Flash Read Write in Quad IO Mode
This example application shows how to use the SST26 SQI flash driver to perform block operations on the On-Board SST26 Flash memory in Quad IO mode.
Description
This application uses the SST26 driver to Erase/Write/Read on the On-Board SST26 Flash memory using the QSPI peripheral library in Quad IO mode.
The application consists of APP_Tasks() which is called through SYS_Tasks() routine.
Downloading and Building the Application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.
Path of the application within the repository is apps/driver/sqi_flash/sst26/sst26_qspi_read_write/firmware.
To build the application, refer to the following table and open the project using its IDE.
| Project Name | Description | 
|---|---|
| wbz653_curiosity.X | MPLABX project for WBZ653 Curiosity Board | 
Setting Up the Hardware
The following table shows the target hardware for the application projects.
| Project Name | Description | 
|---|---|
| wbz653_curiosity.X | WBZ653 Curiosity Board | 
Setting Up WBZ653 Curiosity Board
- Make sure the SST26 QSPI flash is connected to the MCU by connecting 0 Ohm resistor on R739, R742, R744, R746, R749 and R752 on the WBZ653 Curiosity Board
- Connect the Debug USB port on the board to the computer using a micro USB cable
Running the Application
- Build and program the application using its IDE
- Reset the device by power cycle
- LED is turned ON when the data read from SST26 flash matches with the data written in it
| Board | LED Name | 
|---|---|
| WBZ653 Curiosity Board | Red LED |