1 Harmony 3 Driver and System Service Application Examples for PIC32CX-BZ6 and PIC32WM-BZ6204 Family
The following applications are provided to demonstrate the typical or interesting usage
            models of one or more drivers, system services and RTOS.
| Name | Description | 
|---|---|
| Console Debug System Service using UART | This example application demonstrates the UART based console and debug system service | 
| FAT File System using NVM Media | This application shows an example of implementing a FAT disk in the device internal Flash memory | 
| FreeRTOS Basic | This example application demonstrates context switching between four tasks of different priorities. Two tasks run periodically while the other two tasks are event driven | 
| I2C Driver Asynchronous - I2C EEPROM | This example application shows how to use the I2C driver in asynchronous mode to perform operations on the EEPROM | 
| SPI Driver Asynchronous - Self Loopback Multi Client | This example demonstrates how to use the SPI driver in asynchronous mode to achieve self-loop back between multiple clients | 
| SST26 SQI Flash Driver - Flash Read Write in Quad IO Mode | This example application shows how to use the SST26 SQI flash driver to perform block operations on the On-Board SST26 Flash memory in Quad IO mode. | 
| Time System Service Multi-client | This example application demonstrates the multi-client system timer functionality | 
| USART Driver Asynchronous - USART Echo | This example echoes the received characters over the console using the USART driver in asynchronous mode | 
| USART Driver Synchronous - USART Echo | This example echoes the received characters over the console using the USART driver in synchronous mode |