5.3 Curiosity Nano Touch Adapter Mounting
Connecting a Curiosity Nano kit to the Curiosity Nano Touch Adapter board can be done in several ways. The most practical way is to insert the headers of the Curiosity Nano microcontroller board to the sockets of the Curiosity Nano Touch Adapter board. It is also possible to skip the header and socket, and solder the Curiosity Nano kit directly to the Curiosity Nano Touch Adapter board.
Aligning the USB connector on the Curiosity Nano kit with the upper edge of the Curiosity Nano Touch Adapter as shown in Figure 5-1 will connect the board correctly.