1.18 EIC Interrupt

This example application demonstrates how to generate interrupt using the EIC on switch press and indicate it through an LED.

Description

The application registers an event callback with EIC Peripheral library and toggles an LED for every switch press event.

Downloading and Building the Application

To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.

Path of the application within the repository is apps/eic/eic_led_on_off/firmware.

To build the application, refer to the following table and open the project using its IDE.

Project Name Description
sam_c21n_xpro.X MPLABX project for SAMC21N Xplained Pro Evaluation Kit

Setting Up the Hardware

The following table shows the target hardware for the application projects.

Project Name Description
sam_c21n_xpro.X SAMC21N Xplained Pro Evaluation Kit

Setting Up SAMC21N Xplained Pro Evaluation Kit

  • Connect the Debug USB port on the board to the computer using a micro USB cable

Running the Application

  1. Build and Program the application using its IDE
  2. LED toggles on every switch release
Following table provides the Switch and LED names:
Board Switch Name LED Name
SAMC21N Xplained Pro Evaluation Kit SW0 LED0