1.46 TCC PWM Generation

This example application shows how to use the TCC to generate a 2 or 3 phase PWM signals for motor control with dead time.

Description

TCC module is configured to generate synchronous 2 or 3 phase PWM signals with dead time. The duty cycle of the PWM signals is updated in the period interrupt handler.

Downloading and Building the Application

To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.

Path of the application within the repository is apps/tcc/tcc_synchronous_pwm_channels/firmware.

To build the application, refer to the following table and open the project using its IDE.

Project Name Description
sam_c21n_xpro.X MPLABX project for SAMC21N Xplained Pro Evaluation Kit

Setting Up the Hardware

The following table shows the target hardware for the application projects.

Project Name Description
sam_c21n_xpro.X SAMC21N Xplained Pro Evaluation Kit

Setting Up SAMC21N Xplained Pro Evaluation Kit

  • Connect the Debug USB port on the board to the computer using a micro USB cable

Running the Application

  1. Build and Program the application using its IDE
  2. Observe the high-side and low-side PWM waveforms on oscilloscope
  3. Observe the dead time between the high side and the low side
  4. Observe the PWM frequency to be 10 kHz
SAMC21N Xplained Pro Evaluation Kit pin details:
Signal Name Pad Pin
ch2-PWMH PA10 Pin 5 of EXT1 connector
ch2-PWML PB12 Pin 7 of EXT1 connector
ch3-PWMH PA11 Pin 6 of EXT1 connector
ch3-PWML PB13 Pin 8 of EXT1 connector