Introduction
This driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of the device's Analog-to-Digital Converter functionality, for the conversion of analog voltages into a corresponding digital form. The following driver Application Programming Interface (API) modes are covered by this manual:
Polled APIs
Callback APIs
The following peripheral is used by this module:
ADC (Analog-to-Digital Converter)
The following devices can use this module:
Atmel | SMART SAM L21/L22
Atmel | SMART SAM C20/C21
The outline of this documentation is as follows: