3 Hardware
The following sections provide the PIC32CZ CA80/CA90 Curiosity Ultra development board schematics.
Note: This Curiosity Ultra development board
is designed to provide a demonstration platform for as many of the capabilities of the
MCU as possible. Some of the signal multiplexing implemented to accomplish this end is
not recommended for use in customer designs. Specifically in this design, the signals
for the graphics interface and the Ethernet PHY overlap out of necessity. This is highly
discouraged in an end user application.