4 Revision History
Revision C - August 2023
The following changes or updates were made in this revision:
- Added a new note regarding a footprint error to the Xplained Pro Standard Extension Header section
- Added a new note regarding signal multiplexing to the Hardware section
Revision B - February 2023
The following changes or updates were made in this revision:
- Updated EV61X20A/EV16W43A with a new board image
- Updated the first paragraph in Power Block Diagram with new verbiage for powering the board
- Updated Figure 2-5 in Recovery Method with a new image
Revision A - December 2022
This is the initial released version of this document.