3.2.1 Detailed Description

Holds the initial and run-time values of all the parameters required for interrupt frequency diagnosis performed by the DIAG_INT_Frequency function. Initially, for each interrupt that is registered and monitored for the frequency test, the structure parameters are initialized with user-defined values received in the DIAG_INT_FrequencyRegister API. Later, when the test is running, parameters are continuously updated to hold the actual values to be used to evaluate the test.

The documentation for this struct was generated from the following file:

source/

diag_int_frequency.c