2.1.2.2 DIAG_INT_FrequencyGetResult()
diag_result_t DIAG_INT_FrequencyGetResult (diag_int_id_t intId)
Returns the result frequency diagnosis for the required interrupt. The result is set to DIAG_UNDEFINED after returning PASS or FAIL to ensure that the latest result from the diagnostic is returned.
Call the DIAG_INT_FrequencyIsResultReady function to determine if the diagnosis result is ready. |
in | intId |
- ID of the interrupt for which test status is to be obtained |
DIAG_PASS - Success DIAG_FAIL - Failure DIAG_INVALID_ARG - Invalid input arguments when calling the function DIAG_UNDEFINED - Result not ready |