1.8 SPI EEPROM Driver - AT25 EEPROM Read Write

This example application demonstrates how to use the AT25 driver to perform read and write operations on AT25 series of EEPROM.

Description

This example uses the AT25 driver to communicate with the SPI based AT25 series of external EEPROMs to perform read and write operations.

The application communicates with the EEPROM 4 click board that has AT25M02 EEPROM on it.

Downloading and Building the Application

To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.

Path of the application within the repository is apps/driver/spi_eeprom/at25/at25_eeprom_read_write/firmware.

To build the application, refer to the following table and open the project using its IDE.

Project NameDescription
pic32cx_mtsh_db.XMPLABX project for PIC32CXMTSH-DB Evaluation Kit

Setting Up the Hardware

The following table shows the target hardware for the application projects.

Project NameDescription
pic32cx_mtsh_db.X

Running the Application

  1. Build and program the application using its IDE.
  2. The LED indicates success or failure.
    • The LED is turned ON when the value read from EEPROM matches with the written data
Refer to the following table for LED name: