1 Harmony 3 Driver, System Services and RTOS Application Examples for PIC32CX MT Family

The following applications are provided to demonstrate the typical or interesting usage models of driver, system services and RTOS.
NameDescription
Console Debug System Service using UARTThis example application demonstrates the UART based console and debug system service
FAT File System using NVM MediaThis application shows an example of implementing a FAT disk in the device internal Flash memory
FAT File System using SDSPI MediaThis application shows an example of using the FAT File System to access and modify the contents of a SD card using the SDSPI driver and the SPI PLIB
FreeRTOS BasicThis example application demonstrates context switching between four tasks of different priorities. Two tasks run periodically while the other two tasks are event driven
I2C Driver Asynchronous - I2C Multi-clientThis example application demonstrates the multi-client feature of the asynchronous mode of the I2C driver by communicating with an external EEPROM and a temperature sensor
I2C EEPROM Driver - AT24 EEPROM Read WriteThis example application demonstrates how to use the AT24 driver to perform read and write operations on AT24 series of EEPROM
SPI Driver Asynchronous - Self Loopback Multi ClientThis example demonstrates how to use the SPI driver in asynchronous mode to achieve self-loop back between multiple clients
SPI EEPROM Driver - AT25 EEPROM Read WriteThis example application demonstrates how to use the AT25 driver to perform read and write operations on AT25 series of EEPROM
SST26 SQI Flash Driver - Flash Read Write in Quad IO ModeThis example application shows how to use the SST26 SQI flash driver to perform block operations on the On-Board SST26 Flash memory in Quad IO mode.
Time System Service Multi-clientThis example application demonstrates the multi-client system timer functionality
USART Driver Synchronous - Usart EchoThis example application demonstrates the synchronous mode of the USART driver by echoing the received characters