3.3 Moving Data and Code Sections
Unlike the AVR GCC compiler, which typically produces a single .text,
.data and .bss output section, this is not the
case when using MPLAB XC8. Using the --section-start option to move
code and data with MPLAB XC8 will not work reliably.
Description
One consequence of the best-fit allocator (BFA) employed by MPLAB XC8 is that most
objects and code are not placed in the standard .text,
.data and .bss output sections . The compiler
only maps the vector table, .dinit table and some special sections
into the .text output section, leaving other
.text* input sections unmapped. The linker implementation then
creates an output section for each unmapped input section and proceeds to allocate
them as it sees fit.
If you need to explicitly locate any of these standard sections, the
-Wl,--section-start option will not work as expected.
Additionally, any tools used to dump or analyze the output after linking and that
expect to see a single .text section for all the program code might
also fail.
Provided you are using the latest MPLAB XC8 compiler, the
-Wl,--section-start option can be used to position sections
with a user-defined name (sections not called .text,
.data and .bss) and without any modification
to the linker script. User-defined sections can be created using the
__section() specifier.
Migration
The -Wl,-Tsection=addr option can
instead be used to position standard sections, like the .text,
.data and .bss sections at the specified
address.
Although the -Wl,-Ttext option will move the .text
section to the offset specified, this option also sets the starting address from
which the linker begins program memory allocation for all code (even that handled by
the BFA). Thus, when this option is used, the .text section will
start at the exact offset specified; other code sections will be located after this.
Similarly, the -Wl,-Tdata option also sets the starting address
from which the linker begins data (both initialized and uninitialized)
allocation.