1.2 I2C Driver Asynchronous - Multi Client
This example application demonstrates the multi-client feature of the asynchronous mode of the I2C driver by communicating with an external EEPROM and a temperature sensor.
Description
This example uses the I2C driver in asynchronous mode and demonstrates the multi-client feature. The example uses a IO1 Xplained Pro Extension Kit that has a temperature sensor and an EEPROM, both interfaced on the same I2C bus.
Two application tasks are created which act as clients to the same instance of the I2C driver:
- APP_I2C_TEMP_SENSOR_Tasks:
- Reads temperature every 1 second, prints on console and notifies the EEPROM client
 - The Time System Service is used to generate a callback every 1 second
 
 - APP_I2C_EEPROM_Tasks:
- Writes temperature values to the EEPROM once the temperature read complete notification is received
 - The task also reads and prints the last five saved temperature data from the EEPROM when user enters any key on the console
 
 
Downloading and Building the Application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.
Path of the application within the repository is apps/driver/i2c/async/i2c_multi_slave/firmware.
To build the application, refer to the following table and open the project using its IDE.
| Project Name | Description | 
|---|---|
| sam_ha1_xpro.X | MPLABX project for SAM HA1G16A Xplained Pro Evaluation Kit | 
Setting Up the Hardware
The following table shows the target hardware for the application projects.
| Project Name | Description | 
|---|---|
| sam_ha1_xpro.X | SAM HA1G16A Xplained Pro Evaluation Kit | 
Setting Up SAM HA1G16A Xplained Pro Evaluation Kit
To run the demo, the following additional hardware are required:
- IO1 Xplained Pro Extension Kit
 - The A2 address line of TWI must be soldered to GND. This is done to modify
                        the address of the the EEPROM on IO1 Xplained Pro Extension Kit. The
                        modification changes the address of the temperature sensor to 0x4B and the
                        EEPROM to 0x50

 - Connect the IO1 Xplained Pro Extension Kit to the EXT1 header of the SAM HA1G16A Xplained Pro Evaluation Kit
 - Connect the Debug USB port on the board to the computer using a micro USB
                            cableNote: ATSAMHA1G16A device in SAM HA1G16A Xplained Pro board is not recommended for new design, hence replace the device with ATSAMHA1G16AB device. Connect the supported external debugger to Cortex Debug Port.
 
Running the Application
- Open the Terminal application (Ex.:Tera term) on the computer. Configure the
                    DEBUG port settings as follows:
- Baud : 115200
 - Data : 8 Bits
 - Parity : None
 - Stop : 1 Bit
 - Flow Control : None
 
 - Build and program the application using its IDE.
 - Observe the temperature values getting printed on the terminal application every 1 second and temperature value written into EEPROM notification as shown below:
 - Press any key on the terminal, last 5 temperature values will be read from the
                    EEPROM and displayed as shown below.