33.3.2.1 UPDI Enabling
Depending on how the application has configured the UPDI pin, one of the following two methods can be
used to enable the UPDI:
- One-Wire Enable -
This method requires the UPDI pin to be configured in UPDI function
mode by setting the UPDIPINCFG bit in the SYSCFG0 register to
‘
1’. - HV Override of UPDI
Pin - This method is used if the UPDI pin is configured in
GPIO mode (the UPDIPINCFG bit in SYSCFG0 is set to
‘
0’). Applying an HV pulse on RESET will reconfigure the UPDI pin to UPDI function mode, thereby overriding the configuration in the SYSCFG0 fuse.