32.3.3.7.1 Single Conversion
The figure below shows the timing diagram for the ADC when running in Single 8- or 10-bit mode.
Note:
- In Single 8-bit mode, the length of the Conversion state is eight CLK_ADC cycles. In all other modes, it is ten cycles.
- The time from the conversion has finished to the outputs are available in the registers is 0.5 CLK_ADC cycles followed by one CLK_MAIN cycle. With a minimum prescaler of two, this sums up to the maximum of one CLK_ADC cycle.
- If the Low Latency (LOWLAT) bit is set to ‘
1’ in the Control A (ADCn.CTRLA) register, the analog modules in the ADC will not turn OFF at the end of the conversion, which will eliminate the initialization time when triggering the following conversion.
The total conversion time for a single result is calculated by:
If the Free-Running (FREERUN) bit is set to
‘1’ in the Control F (ADCn.CTRLF) register, a new conversion will be
started immediately after a result is available in the Result (ADCn.RESULT) register. The
Free-Running conversion rate (fconv) is calculated by: