1 Hardware Requirements
The Data Logging example application requires the following hardware:
XMEGA A1U Xplained Pro Evaluation Kit which includes:
- Atmel ATxmega128A1U microcontroller
- One mechanical reset button
- One mechanical user push-button
- One yellow user LED
- 32.768kHz crystal
- External 512KB SRAM
- USB interface, device mode
- Three Xplained Pro extension headers
- Xplained Pro LCD extension connector
- Embedded Debugger
- USB powered
For more details of XMEGA A1U Xplained Pro Evaluation Kit, refer to http://www.atmel.com/tools/atxmegaa1u-xpro.aspx and XMEGA A1U Xplained Pro User Guide.
This example can also be easily ported to other XMEGA devices.