Jump to main content
30.4.2.4 Synchronous Client Reception Setup
- Set the SYNC and SPEN bits and clear the CSRC bit.
- Select the receive input pin by writing the appropriate value to the RXxPPS
register.
- Select the clock input pin by writing
the appropriate values to the TXxPPS register.
- Clear the ANSEL bit for both the TXx/CKx and RXx/DTx pins (if
applicable).
- If interrupts are desired, set the RCxIE bit of the PIEx
register and the GIE and PEIE bits of the INTCON register.
- If 9-bit reception is desired, set the RX9
bit.
- Set the CREN bit to enable reception.
- The RCxIF bit will be set when reception is complete. An interrupt will be generated if the RCxIE bit was set.
- If 9-bit mode is enabled, retrieve the Most Significant bit from
the RX9D bit.
- Retrieve the eight Least Significant bits from the receive FIFO
by reading the RCxREG register.
- If an overrun error occurs, clear the error by either clearing
the CREN bit or by clearing the SPEN bit which resets the EUSART.