3.10.2 NVMCTRL with BOOTEND and APPEND
Nonvolatile Memory Controller with BOOTEND and APPEND
3.10.2.1 Introduction
This NVM Controller (NVMCTRL) Module is the interface between the CPU and Nonvolatile Memories (Flash, EEPROM, Signature Row, User Row and fuses). These are reprogrammable memory blocks that retain their values even when they are not powered. The Flash is mainly used for program storage and can also be used for data storage. The EEPROM is used for data storage and can be programmed while the CPU is running the program from the Flash. The sizes of the sections in the Flash section can be set by the Boot Section End fuse and the Application Section End fuse
3.10.2.2 Supported Device Families
ATtiny | ATmega16xx | ATmega48xx |
ATmega80x | ATmega88xx |
3.10.2.3 Required header files:
#include "mcc_generated_files/nvm/nvm.h"
3.10.2.4 How to use the Memory drivers
The Memory driver can be used to access different types of memory. Click the links below to view examples on how to access the Flash and EEPROM memory.
- Accessing the Flash Memory
- Accessing the EEPROM Memory
- Accessing SIGROW
- Accessing the Fuse
3.10.2.5 Module Documentation
3.10.2.5.1 Non-Volatile Memory
This file contains API prototypes and other data types for the Non-Volatile Memory (NVM) driver.
Module description
This file contains API prototypes and other data types for the Non-Volatile Memory (NVM) driver.
Typedefs
typedef uint8_t flash_data_t
Data type for the Flash data.
typedef uint16_t flash_address_t
Data type for the Flash address.
typedef uint8_t eeprom_data_t
Data type for the EEPROM data.
typedef uint16_t eeprom_address_t
Data type for the EEPROM address.
typedef uint8_t sigrow_data_t
Data type for the Signature Row data.
typedef uint16_t sigrow_address_t
Datatype for Signature Row address.
typedef uint32_t device_id_data_t
Data type for the Device ID data.
typedef uint8_t fuse_data_t
Data type for the Fuse data.
typedef uint16_t fuse_address_t
Data type for the Fuse address.
typedef uint8_t flash_data_t
Data type for the Flash data.
typedef uint16_t flash_address_t
Data type for the Flash address.
typedef uint8_t eeprom_data_t
Data type for the EEPROM data.
typedef uint16_t eeprom_address_t
Data type for the EEPROM address.
typedef uint8_t sigrow_data_t
Data type for the Signature Row data.
typedef uint16_t sigrow_address_t
Datatype for Signature Row address.
typedef uint32_t device_id_data_t
Data type for the Device ID data.
typedef uint8_t fuse_data_t
Data type for the Fuse data.
typedef uint16_t fuse_address_t
Data type for the Fuse address.
Definitions
#define PROGMEM_BLOCK_SIZE (256U)
#define SERIAL_NUMBER_SIZE (10U)
#define PROGMEM_BLOCK_SIZE (256U)
#define SERIAL_NUMBER_SIZE (10U)
Enumerations
enum nvm_status_t { NVM_OK, NVM_ERROR, NVM_OK, NVM_ERROR }
Contains the return codes for the NVM driver APIs.
Functions
void NVM_Initialize (void)
Initializes the NVM driver.
nvm_status_t NVM_StatusGet (void)
Returns the status of the last NVM operation.
flash_data_t FLASH_Read (flash_address_t address)
Reads a byte from the given Flash address.
nvm_status_t FLASH_RowWrite (flash_address_t address, flash_data_t *dataBuffer)
Writes one entire Flash row/page from the given starting address of the row (the first byte location). The size of the input buffer must be one Flash row and the address must be aligned with the row boundary. Use FLASH_PageAddressGet() to obtain the starting address of the row.
nvm_status_t FLASH_PageErase (flash_address_t address)
Erases one Flash page containing the given address.
flash_address_t FLASH_PageAddressGet (flash_address_t address)
Returns the starting address of the page (the first byte location) containing the given Flash address.
uint16_t FLASH_PageOffsetGet (flash_address_t address)
Returns the offset from the starting address of the page (the first byte location).
bool FLASH_IsBusy (void)
Checks if the Flash is busy.
eeprom_data_t EEPROM_Read (eeprom_address_t address)
Reads one byte from the given EEPROM address.
void EEPROM_Write (eeprom_address_t address, eeprom_data_t data)
Writes one byte to the given EEPROM address. The EEPROM busy status must be checked using the EEPROM_IsBusy() API to know if the write operation is completed.
bool EEPROM_IsBusy (void)
Checks if the EEPROM is busy.
void EEPROM_ReadyInterruptEnable (void)
Enables the EEREADY interrupt.
void EEPROM_ReadyInterruptDisable (void)
Disables the EEREADY interrupt.
void EEPROM_CallbackRegister (void(*CallbackHandler)(void))
Setter function for the EEPROM Ready interrupt callback.
sigrow_data_t SIGROW_Read (sigrow_address_t address)
Reads one Signature Row byte.
device_id_data_t SIGROW_DeviceIDRead (sigrow_address_t address)
Reads the Device ID.
void SIGROW_SerialNumberRead (sigrow_address_t address, sigrow_data_t *serialNumber)
Reads the serial number. The size of the buffer must be equal to the size of the serial number.
fuse_data_t FUSE_Read (fuse_address_t address)
Reads a fuse.
Definition Documentation
PROGMEM_BLOCK_SIZE[1/2]
#define PROGMEM_BLOCK_SIZE (256U)
Contains the program memory block size in bytes. The BOOTEND and APPEND fuses select the Flash section sizes in blocks of PROGMEM_BLOCK_SIZE bytes.
PROGMEM_BLOCK_SIZE[1/2]
#define PROGMEM_BLOCK_SIZE (256U)
Contains the program memory block size in bytes. The BOOTEND and APPEND fuses select the Flash section sizes in blocks of PROGMEM_BLOCK_SIZE bytes.
SERIAL_NUMBER_SIZE[1/2]
#define SERIAL_NUMBER_SIZE (10U)
Contains the serial number length in bytes.
SERIAL_NUMBER_SIZE[1/2]
#define SERIAL_NUMBER_SIZE (10U)
Contains the serial number length in bytes.
Typedef Documentation
device_id_data_t[1/2]
typedef uint32_t device_id_data_t
Data type for the Device ID data.
device_id_data_t[1/2]
typedef uint32_t device_id_data_t
Data type for the Device ID data.
eeprom_address_t[1/2]
typedef uint16_t eeprom_address_t
Data type for the EEPROM address.
eeprom_address_t[1/2]
typedef uint16_t eeprom_address_t
Data type for the EEPROM address.
eeprom_data_t[1/2]
typedef uint8_t eeprom_data_t
Data type for the EEPROM data.
eeprom_data_t[1/2]
typedef uint8_t eeprom_data_t
Data type for the EEPROM data.
flash_address_t[1/2]
typedef uint16_t flash_address_t
Data type for the Flash address.
flash_address_t[1/2]
typedef uint16_t flash_address_t
Data type for the Flash address.
flash_data_t[1/2]
typedef uint8_t flash_data_t
Data type for the Flash data.
flash_data_t[1/2]
typedef uint8_t flash_data_t
Data type for the Flash data.
fuse_address_t[1/2]
typedef uint16_t fuse_address_t
Data type for the Fuse address.
fuse_address_t[1/2]
typedef uint16_t fuse_address_t
Data type for the Fuse address.
fuse_data_t[1/2]
typedef uint8_t fuse_data_t
Data type for the Fuse data.
fuse_data_t[1/2]
typedef uint8_t fuse_data_t
Data type for the Fuse data.
sigrow_address_t[1/2]
typedef uint16_t sigrow_address_t
Datatype for Signature Row address.
sigrow_address_t[1/2]
typedef uint16_t sigrow_address_t
Datatype for Signature Row address.
sigrow_data_t[1/2]
typedef uint8_t sigrow_data_t
Data type for the Signature Row data.
sigrow_data_t[1/2]
typedef uint8_t sigrow_data_t
Data type for the Signature Row data.
Function Documentation
EEPROM_CallbackRegister()
void EEPROM_CallbackRegister (void(*)(void) CallbackHandler)
Setter function for the EEPROM Ready interrupt callback.
|
None. |
EEPROM_IsBusy()
bool EEPROM_IsBusy (void )
Checks if the EEPROM is busy.
NVM must be initialized with NVM_Initialize() before calling this API. |
|
|
EEPROM_Read()
eeprom_data_t EEPROM_Read (eeprom_address_t address)
Reads one byte from the given EEPROM address.
NVM must be initialized with NVM_Initialize() before calling this API. |
|
Byte read from the given EEPROM address. |
EEPROM_ReadyInterruptDisable()
void EEPROM_ReadyInterruptDisable (void )[inline]
Disables the EEREADY interrupt.
The interrupt can be disabled in the interrupt handler. |
|
None. |
EEPROM_ReadyInterruptEnable()
void EEPROM_ReadyInterruptEnable (void )[inline]
Enables the EEREADY interrupt.
The interrupt must be enabled only after triggering a NVM command. Global interrupt must be enabled for the EERADY interrupt to work. |
|
None. |
EEPROM_Write()
void EEPROM_Write (eeprom_address_t address, eeprom_data_t data)
Writes one byte to the given EEPROM address. The EEPROM busy status must be checked using the EEPROM_IsBusy() API to know if the write operation is completed.
|
None. |
FLASH_IsBusy()
bool FLASH_IsBusy (void )
Checks if the Flash is busy.
NVM must be initialized with NVM_Initialize() before calling this API. |
|
|
FLASH_PageAddressGet()
flash_address_t FLASH_PageAddressGet (flash_address_t address)
Returns the starting address of the page (the first byte location) containing the given Flash address.
|
Starting address of the page containing the given Flash address. |
FLASH_PageErase()
nvm_status_t FLASH_PageErase (flash_address_t address)
Erases one Flash page containing the given address.
NVM must be initialized with NVM_Initialize() before calling this API. |
|
Status of the Flash page erase operation as described in nvm_status_t. |
FLASH_PageOffsetGet()
uint16_t FLASH_PageOffsetGet (flash_address_t address)
Returns the offset from the starting address of the page (the first byte location).
|
Offset of the given address from the starting address of the page. |
FLASH_Read()
flash_data_t FLASH_Read (flash_address_t address)
Reads a byte from the given Flash address.
NVM must be initialized with NVM_Initialize() before calling this API. |
|
Byte read from the given Flash address. |
FLASH_RowWrite()
nvm_status_t FLASH_RowWrite (flash_address_t address, flash_data_t * dataBuffer)
Writes one entire Flash row/page from the given starting address of the row (the first byte location). The size of the input buffer must be one Flash row and the address must be aligned with the row boundary. Use FLASH_PageAddressGet() to obtain the starting address of the row.
Erase Flash row before calling this function. |
|
Status of the Flash row write operation as described in nvm_status_t. |
FUSE_Read()
fuse_data_t FUSE_Read (fuse_address_t address)
Reads a fuse.
|
Fuse data. |
NVM_Initialize()
void NVM_Initialize (void )
Initializes the NVM driver.
|
None. |
NVM_StatusGet()
nvm_status_t NVM_StatusGet (void )
Returns the status of the last NVM operation.
|
|
SIGROW_DeviceIDRead()
device_id_data_t SIGROW_DeviceIDRead (sigrow_address_t address)
Reads the Device ID.
|
Device ID. |
SIGROW_Read()
sigrow_data_t SIGROW_Read (sigrow_address_t address)
Reads one Signature Row byte.
|
Signature Row data. |
SIGROW_SerialNumberRead()
void SIGROW_SerialNumberRead (sigrow_address_t address, sigrow_data_t * serialNumber)
Reads the serial number. The size of the buffer must be equal to the size of the serial number.
|
None. |
Enumeration Type Documentation
nvm_status_t
enum nvm_status_t
Contains the return codes for the NVM driver APIs.
NVM_OK |
0 - The NVM operation succeeded. | |
NVM_ERROR |
1 - The NVM operation failed. | |
NVM_OK |
0 - The NVM operation succeeded. | |
NVM_ERROR |
1 - The NVM operation failed. |
3.10.2.5.2 Nvm_example
Flash Examples
This example shows how to overwrite an entire Flash page with the new data using the row write feature:
#include "mcc_generated_files/system/system.h" #define FLASH_ADDRESS (PROGMEM_SIZE - 5) //Flash address at which data is to be written void FLASH_Example_PageErase_RowWrite_Read(void) { flash_address_t flashStartPageAddress; uint16_t index; flash_data_t flashWriteData[PROGMEM_PAGE_SIZE]; bool readError = false; //Get the starting address of the page containing the given address flashStartPageAddress = FLASH_PageAddressGet(FLASH_ADDRESS); //Erase the entire page if (FLASH_PageErase(flashStartPageAddress) == NVM_OK) { printf("FLASH_PageErase passed \r\n"); } else { printf("FLASH_PageErase failed \r\n"); } //Prepare the row data for (index = 0; index < PROGMEM_PAGE_SIZE; index++) { flashWriteData[index] = (flash_data_t) index; } //Write data to the Flash row if (FLASH_RowWrite(flashStartPageAddress, flashWriteData) == NVM_OK) { printf("FLASH_RowWrite passed \r\n"); } else { printf("FLASH_RowWrite failed \r\n"); } //Read and verify the row data for (index = 0; index < PROGMEM_PAGE_SIZE; index++) { if (FLASH_Read(flashStartPageAddress + index) != flashWriteData[index]) { readError = true; break; } } if (readError == false) { printf("FLASH_Read passed \r\n"); } else { printf("FLASH_Read failed \r\n"); } }
This example shows how to update the specific locations in a given Flash page without disturbing the other locations:
#include "mcc_generated_files/system/system.h" #define FLASH_ADDRESS (PROGMEM_SIZE - 5) //Flash address at which data is to be written void FLASH_Example_UpdateSelectiveLocations(void) { flash_address_t flashStartPageAddress; uint16_t flashAddressOffset; flash_data_t flashWriteData[PROGMEM_PAGE_SIZE]; nvm_status_t errorStatus = NVM_OK; bool readError = false; //Get the starting address of the page containing the given address flashStartPageAddress = FLASH_PageAddressGet(FLASH_ADDRESS); //Read the entire row for (flashAddressOffset = 0; flashAddressOffset < PROGMEM_PAGE_SIZE; flashAddressOffset++) { flashWriteData[flashAddressOffset] = FLASH_Read(flashStartPageAddress + flashAddressOffset); } //Get offset from the starting address of the page flashAddressOffset = FLASH_PageOffsetGet(FLASH_ADDRESS); //Update 4 bytes flashWriteData[flashAddressOffset] = 0xA0; flashWriteData[flashAddressOffset + 1] = 0xA1; flashWriteData[flashAddressOffset + 2] = 0xA2; flashWriteData[flashAddressOffset + 3] = 0xA3; //Erase the entire Flash page if (FLASH_PageErase(flashStartPageAddress) == NVM_OK) { printf("FLASH_PageErase passed \r\n"); } else { printf("FLASH_PageErase failed \r\n"); } //Write data to the Flash row errorStatus = FLASH_RowWrite(flashStartPageAddress, flashWriteData); if (errorStatus == NVM_OK) { printf("FLASH_RowWrite passed \r\n"); } else { printf("FLASH_RowWrite failed \r\n"); } //Read and verify the row data for (flashAddressOffset = 0; flashAddressOffset < PROGMEM_PAGE_SIZE; flashAddressOffset++) { //Verify if (FLASH_Read(flashStartPageAddress + flashAddressOffset) != flashWriteData[flashAddressOffset]) { readError = true; break; } } if (readError == false) { printf("FLASH_Read passed \r\n"); } else { printf("FLASH_Read failed \r\n"); } }
EEPROM Examples
This example shows how to perform the write and read operations on EEPROM:
#include "mcc_generated_files/system/system.h" #define EEPROM_ADDRESS (EEPROM_START) //EEPROM address at which data is to be written void EEPROM_Write_Read(void) { eeprom_data_t eepromWriteData[8]; uint8_t count; bool readError = false; //Prepare the data for (count = 0; count < 8; count++) { eepromWriteData[count] = 0xA1 + count; } for (count = 0; count < 8; count++) { //Write EEPROM byte EEPROM_Write(EEPROM_ADDRESS + count, eepromWriteData[count]); while (EEPROM_IsBusy()); if (NVM_StatusGet() == NVM_OK) { printf("EEPROM_Write passed \r\n"); } else { printf("EEPROM_Write failed \r\n"); } } //Read and verify for (count = 0; count < 8; count++) { if (EEPROM_Read(EEPROM_ADDRESS + count) != eepromWriteData[count]) { readError = true; break; } } if (readError == false) { printf("EEPROM_Read passed \r\n"); } else { printf("EEPROM_Read failed \r\n"); } }
SIGROW Examples
This example shows how to read the Signature Row:
#include "mcc_generated_files/system/system.h" #define SIGROW_START_ADDRESS (0x1100U) //Compare with the device data sheet to see if the address is correct #define SIGROW_END_ADDRESS (0x111FU) //Compare with the device data sheet to see if the address is correct void NVM_Example_Signature_Row_Read_All(void) { sigrow_address_t address; for (address = SIGROW_START_ADDRESS; address <= SIGROW_END_ADDRESS; address++) { printf(" 0x%X \r\n", SIGROW_Read(address)); } }
This example shows how to read the Device ID:
#include "mcc_generated_files/system/system.h" #define DEVICE_ID_ADDRESS (0x1100U) void NVM_Example_DeviceID_Read(void) { printf("Device ID : 0x%lX \r\n", SIGROW_DeviceIDRead(DEVICE_ID_ADDRESS)); }
This example shows how to read the Serial Number:
#include "mcc_generated_files/system/system.h" #define SERIAL_NUMBER_START_ADDRESS (0x1103U) //Compare with the device data sheet to see if the address is correct void NVM_Example_Serial_Number_Read(void) { sigrow_address_t address = SERIAL_NUMBER_START_ADDRESS; sigrow_data_t NVM_SerialNumberReadData[SERIAL_NUMBER_SIZE]; uint8_t serialNumberIndex; SIGROW_SerialNumberRead(address, NVM_SerialNumberReadData); for (serialNumberIndex = 0; serialNumberIndex < SERIAL_NUMBER_SIZE; serialNumberIndex++) { printf("Serial Number %u : 0x%X \r\n", serialNumberIndex , NVM_SerialNumberReadData[serialNumberIndex]); } }
Fuse Examples
This example shows how to read the Fuse:
#include "mcc_generated_files/system/system.h" #define FUSE_START_ADDRESS (0x1280U) //Compare with the device data sheet to see if the address is correct #define FUSE_END_ADDRESS (0x1288U) //Compare with the device data sheet to see if the address is correct void NVM_Example_Fuse_Read_All(void) { fuse_address_t address; for (address = FUSE_START_ADDRESS; address <= FUSE_END_ADDRESS; address++) { printf("0x%X \r\n", FUSE_Read(address)); } }
3.10.2.6 File Documentation
3.10.2.6.1 source/nvm_example.dox File Reference
3.10.2.6.2 source/nvm_interrupt.c File Reference
#include "../../system/ccp.h" #include "../nvm.h"
Functions
void NVM_Initialize (void)
Initializes the NVM driver.
nvm_status_t NVM_StatusGet (void)
Returns the status of the last NVM operation.
flash_data_t FLASH_Read (flash_address_t address)
Reads a byte from the given Flash address.
nvm_status_t FLASH_RowWrite (flash_address_t address, flash_data_t *dataBuffer)
Writes one entire Flash row/page from the given starting address of the row (the first byte location). The size of the input buffer must be one Flash row and the address must be aligned with the row boundary. Use FLASH_PageAddressGet() to obtain the starting address of the row.
nvm_status_t FLASH_PageErase (flash_address_t address)
Erases one Flash page containing the given address.
flash_address_t FLASH_PageAddressGet (flash_address_t address)
Returns the starting address of the page (the first byte location) containing the given Flash address.
uint16_t FLASH_PageOffsetGet (flash_address_t address)
Returns the offset from the starting address of the page (the first byte location).
bool FLASH_IsBusy (void)
Checks if the Flash is busy.
eeprom_data_t EEPROM_Read (eeprom_address_t address)
Reads one byte from the given EEPROM address.
void EEPROM_Write (eeprom_address_t address, eeprom_data_t data)
Writes one byte to the given EEPROM address. The EEPROM busy status must be checked using the EEPROM_IsBusy() API to know if the write operation is completed.
bool EEPROM_IsBusy (void)
Checks if the EEPROM is busy.
void EEPROM_ReadyInterruptEnable (void)
Enables the EEREADY interrupt.
void EEPROM_ReadyInterruptDisable (void)
Disables the EEREADY interrupt.
ISR (NVMCTRL_EE_vect)
void EEPROM_CallbackRegister (void(*CallbackHandler)(void))
Setter function for the EEPROM Ready interrupt callback.
sigrow_data_t SIGROW_Read (sigrow_address_t address)
Reads one Signature Row byte.
device_id_data_t SIGROW_DeviceIDRead (sigrow_address_t address)
Reads the Device ID.
void SIGROW_SerialNumberRead (sigrow_address_t address, sigrow_data_t *serialNumber)
Reads the serial number. The size of the buffer must be equal to the size of the serial number.
fuse_data_t FUSE_Read (fuse_address_t address)
Reads a fuse.
Variables
static void(* EEPROM_Callback )(void) = NULL
Function Documentation
ISR()
ISR (NVMCTRL_EE_vect )
Variable Documentation
EEPROM_Callback
void(* EEPROM_Callback) (void) = NULL[static]
3.10.2.6.3 source/nvm_interrupt.h File Reference
#include "../system/utils/compiler.h"
Functions
void NVM_Initialize (void)
Initializes the NVM driver.
nvm_status_t NVM_StatusGet (void)
Returns the status of the last NVM operation.
flash_data_t FLASH_Read (flash_address_t address)
Reads a byte from the given Flash address.
nvm_status_t FLASH_RowWrite (flash_address_t address, flash_data_t *dataBuffer)
Writes one entire Flash row/page from the given starting address of the row (the first byte location). The size of the input buffer must be one Flash row and the address must be aligned with the row boundary. Use FLASH_PageAddressGet() to obtain the starting address of the row.
nvm_status_t FLASH_PageErase (flash_address_t address)
Erases one Flash page containing the given address.
flash_address_t FLASH_PageAddressGet (flash_address_t address)
Returns the starting address of the page (the first byte location) containing the given Flash address.
uint16_t FLASH_PageOffsetGet (flash_address_t address)
Returns the offset from the starting address of the page (the first byte location).
bool FLASH_IsBusy (void)
Checks if the Flash is busy.
eeprom_data_t EEPROM_Read (eeprom_address_t address)
Reads one byte from the given EEPROM address.
void EEPROM_Write (eeprom_address_t address, eeprom_data_t data)
Writes one byte to the given EEPROM address. The EEPROM busy status must be checked using the EEPROM_IsBusy() API to know if the write operation is completed.
bool EEPROM_IsBusy (void)
Checks if the EEPROM is busy.
void EEPROM_ReadyInterruptEnable (void)
Enables the EEREADY interrupt.
void EEPROM_ReadyInterruptDisable (void)
Disables the EEREADY interrupt.
void EEPROM_CallbackRegister (void(*CallbackHandler)(void))
Setter function for the EEPROM Ready interrupt callback.
sigrow_data_t SIGROW_Read (sigrow_address_t address)
Reads one Signature Row byte.
device_id_data_t SIGROW_DeviceIDRead (sigrow_address_t address)
Reads the Device ID.
void SIGROW_SerialNumberRead (sigrow_address_t address, sigrow_data_t *serialNumber)
Reads the serial number. The size of the buffer must be equal to the size of the serial number.
fuse_data_t FUSE_Read (fuse_address_t address)
Reads a fuse.
Macros
#define PROGMEM_BLOCK_SIZE (256U)
#define SERIAL_NUMBER_SIZE (10U)
Typedefs
typedef uint8_t flash_data_t
Data type for the Flash data.
typedef uint16_t flash_address_t
Data type for the Flash address.
typedef uint8_t eeprom_data_t
Data type for the EEPROM data.
typedef uint16_t eeprom_address_t
Data type for the EEPROM address.
typedef uint8_t sigrow_data_t
Data type for the Signature Row data.
typedef uint16_t sigrow_address_t
Datatype for Signature Row address.
typedef uint32_t device_id_data_t
Data type for the Device ID data.
typedef uint8_t fuse_data_t
Data type for the Fuse data.
typedef uint16_t fuse_address_t
Data type for the Fuse address.
Enumerations
enum nvm_status_t { NVM_OK, NVM_ERROR, NVM_OK, NVM_ERROR }
Contains the return codes for the NVM driver APIs.
Macro Definition Documentation
FLASH_ErasePageAddressGet
#define FLASH_ErasePageAddressGet FLASH_PageAddressGet
FLASH_ErasePageOffsetGet
#define FLASH_ErasePageOffsetGet FLASH_PageOffsetGet
3.10.2.6.4 source/nvm_polling.c File Reference
#include "../../system/ccp.h" #include "../nvm.h"
Functions
void NVM_Initialize (void)
Initializes the NVM driver.
nvm_status_t NVM_StatusGet (void)
Returns the status of the last NVM operation.
flash_data_t FLASH_Read (flash_address_t address)
Reads a byte from the given Flash address.
nvm_status_t FLASH_RowWrite (flash_address_t address, flash_data_t *dataBuffer)
Writes one entire Flash row/page from the given starting address of the row (the first byte location). The size of the input buffer must be one Flash row and the address must be aligned with the row boundary. Use FLASH_PageAddressGet() to obtain the starting address of the row.
nvm_status_t FLASH_PageErase (flash_address_t address)
Erases one Flash page containing the given address.
flash_address_t FLASH_PageAddressGet (flash_address_t address)
Returns the starting address of the page (the first byte location) containing the given Flash address.
uint16_t FLASH_PageOffsetGet (flash_address_t address)
Returns the offset from the starting address of the page (the first byte location).
bool FLASH_IsBusy (void)
Checks if the Flash is busy.
eeprom_data_t EEPROM_Read (eeprom_address_t address)
Reads one byte from the given EEPROM address.
void EEPROM_Write (eeprom_address_t address, eeprom_data_t data)
Writes one byte to the given EEPROM address. The EEPROM busy status must be checked using the EEPROM_IsBusy() API to know if the write operation is completed.
bool EEPROM_IsBusy (void)
Checks if the EEPROM is busy.
sigrow_data_t SIGROW_Read (sigrow_address_t address)
Reads one Signature Row byte.
device_id_data_t SIGROW_DeviceIDRead (sigrow_address_t address)
Reads the Device ID.
void SIGROW_SerialNumberRead (sigrow_address_t address, sigrow_data_t *serialNumber)
Reads the serial number. The size of the buffer must be equal to the size of the serial number.
fuse_data_t FUSE_Read (fuse_address_t address)
Reads a fuse.
3.10.2.6.5 source/nvm_polling.h File Reference
#include "../system/utils/compiler.h"
Functions
void NVM_Initialize (void)
Initializes the NVM driver.
nvm_status_t NVM_StatusGet (void)
Returns the status of the last NVM operation.
flash_data_t FLASH_Read (flash_address_t address)
Reads a byte from the given Flash address.
nvm_status_t FLASH_RowWrite (flash_address_t address, flash_data_t *dataBuffer)
Writes one entire Flash row/page from the given starting address of the row (the first byte location). The size of the input buffer must be one Flash row and the address must be aligned with the row boundary. Use FLASH_PageAddressGet() to obtain the starting address of the row.
nvm_status_t FLASH_PageErase (flash_address_t address)
Erases one Flash page containing the given address.
flash_address_t FLASH_PageAddressGet (flash_address_t address)
Returns the starting address of the page (the first byte location) containing the given Flash address.
uint16_t FLASH_PageOffsetGet (flash_address_t address)
Returns the offset from the starting address of the page (the first byte location).
bool FLASH_IsBusy (void)
Checks if the Flash is busy.
eeprom_data_t EEPROM_Read (eeprom_address_t address)
Reads one byte from the given EEPROM address.
void EEPROM_Write (eeprom_address_t address, eeprom_data_t data)
Writes one byte to the given EEPROM address. The EEPROM busy status must be checked using the EEPROM_IsBusy() API to know if the write operation is completed.
bool EEPROM_IsBusy (void)
Checks if the EEPROM is busy.
sigrow_data_t SIGROW_Read (sigrow_address_t address)
Reads one Signature Row byte.
device_id_data_t SIGROW_DeviceIDRead (sigrow_address_t address)
Reads the Device ID.
void SIGROW_SerialNumberRead (sigrow_address_t address, sigrow_data_t *serialNumber)
Reads the serial number. The size of the buffer must be equal to the size of the serial number.
fuse_data_t FUSE_Read (fuse_address_t address)
Reads a fuse.
Macros
#define PROGMEM_BLOCK_SIZE (256U)
#define SERIAL_NUMBER_SIZE (10U)
Typedefs
typedef uint8_t flash_data_t
Data type for the Flash data.
typedef uint16_t flash_address_t
Data type for the Flash address.
typedef uint8_t eeprom_data_t
Data type for the EEPROM data.
typedef uint16_t eeprom_address_t
Data type for the EEPROM address.
typedef uint8_t sigrow_data_t
Data type for the Signature Row data.
typedef uint16_t sigrow_address_t
Datatype for Signature Row address.
typedef uint32_t device_id_data_t
Data type for the Device ID data.
typedef uint8_t fuse_data_t
Data type for the Fuse data.
typedef uint16_t fuse_address_t
Data type for the Fuse address.
Enumerations
enum nvm_status_t { NVM_OK, NVM_ERROR, NVM_OK, NVM_ERROR }
Macro Definition Documentation
FLASH_ErasePageAddressGet
#define FLASH_ErasePageAddressGet FLASH_PageAddressGet
FLASH_ErasePageOffsetGet
#define FLASH_ErasePageOffsetGet FLASH_PageOffsetGet
Enumeration Type Documentation
nvm_status_t
enum nvm_status_t
NVM_OK |
0 - The NVM operation succeeded. | |
NVM_ERROR |
1 - The NVM operation failed. | |
NVM_OK |
0 - The NVM operation succeeded. | |
NVM_ERROR |
1 - The NVM operation failed. |