4.5 CHPMP - Charge Pump
4.5.1 Introduction
The MPLAB® Code Configurator (MCC) Melody Charge Pump (CHPMP) Peripheral Library (PLIB) drivers generates APIs to support CHPMP-specific peripheral functionality on target MCUs.
The primary use of the charge pump is to supply a constant voltage to the gates of transistor devices contained in analog peripherals, signal and reference circuitry, and to prevent degradation of transistor performance at low operating voltages.
4.5.2 Supported Device Families
| PIC16F152xx | PIC16F171xx | PIC16F180xx | PIC16F181xx |
4.5.3 Required Header Files
#include "mcc_generated_files/chpmp/chpmp.h"
4.5.4 Module Documentation
4.5.4.1 Chpmp
This file contains the API prototypes for the Charge Pump (CHPMP) driver.
4.5.4.1.1 Module description
This file contains the API prototypes for the Charge Pump (CHPMP) driver.
Definitions
#define myCHPMP_Initialize CHPMP_Initialize
Defines the Custom Name for the CHPMP_Initialize API.
#define myCHPMP_Enable CHPMP_Enable
Defines the Custom Name for the CHPMP_Enable API.
#define myCHPMP_Disable CHPMP_Disable
Defines the Custom Name for the CHPMP_Disable API.
#define myCHPMP_IsVDDAboveVAuto CHPMP_IsVDDAboveVAuto
Defines the Custom Name for the CHPMP_IsVDDAboveVAuto API.
#define myCHPMP_IsReady CHPMP_IsReady
Defines the Custom Name for the CHPMP_IsReady API.
Functions
void CHPMP_Initialize (void)
Initializes the CHPMP module.
void CHPMP_Enable (void)
Enables the CHPMP module.
bool CHPMP_Disable (void)
Disables the CHPMP module. If the return value is False, turn off all analog peripherals and try again.
bool CHPMP_IsVDDAboveVAuto (void)
Returns the status of the CHPMP threshold.
bool CHPMP_IsReady (void)
Returns the status of Steady state.
4.5.4.1.2 Definition Documentation
myCHPMP_Disable
#define myCHPMP_Disable CHPMP_Disable
Defines the Custom Name for the CHPMP_Disable API.
myCHPMP_Enable
#define myCHPMP_Enable CHPMP_Enable
Defines the Custom Name for the CHPMP_Enable API.
myCHPMP_Initialize
#define myCHPMP_Initialize CHPMP_Initialize
Defines the Custom Name for the CHPMP_Initialize API.
Section: Included Files
myCHPMP_IsReady
#define myCHPMP_IsReady CHPMP_IsReady
Defines the Custom Name for the CHPMP_IsReady API.
myCHPMP_IsVDDAboveVAuto
#define myCHPMP_IsVDDAboveVAuto CHPMP_IsVDDAboveVAuto
Defines the Custom Name for the CHPMP_IsVDDAboveVAuto API.
4.5.4.1.3 Function Documentation
CHPMP_Disable()
bool CHPMP_Disable (void )
Disables the CHPMP module. If the return value is False, turn off all analog peripherals and try again.
| None. |
| True |
- Charge pump is disabled |
| False |
- Charge pump has been requested by an analog peripheral |
CHPMP_Enable()
void CHPMP_Enable (void )
Enables the CHPMP module.
| None. |
None. |
CHPMP_Initialize()
void CHPMP_Initialize (void )
Initializes the CHPMP module.
| None. |
None. |
Section: Included Files
CHPMP_IsReady()
bool CHPMP_IsReady (void )
Returns the status of Steady state.
| None. |
| True |
- Steady state is reached |
| False |
- Steady state is not reached |
CHPMP_IsVDDAboveVAuto()
bool CHPMP_IsVDDAboveVAuto (void )
Returns the status of the CHPMP threshold.
| None. |
| True |
- VDD is above the threshold voltage(VAUTO) |
| False |
- VDD is below the threshold voltage(VAUTO) |
4.5.5 File Documentation
4.5.5.1 source/source-files/chpmp.c File Reference
This file contains the API implementations for the Charge Pump (CHPMP) driver.
#include <xc.h> #include "../chpmp.h"
4.5.5.1.1 Functions
void CHPMP_Initialize (void)
Initializes the CHPMP module.
void CHPMP_Enable (void)
Enables the CHPMP module.
bool CHPMP_Disable (void)
Disables the CHPMP module. If the return value is False, turn off all analog peripherals and try again.
bool CHPMP_IsVDDAboveVAuto (void)
Returns the status of the CHPMP threshold.
bool CHPMP_IsReady (void)
Returns the status of Steady state.
4.5.5.1.2 Detailed Description
This file contains the API implementations for the Charge Pump (CHPMP) driver.
CHPMP Generated Driver File
4.5.5.2 source/source-files/chpmp.h File Reference
#include <stdbool.h> #include <stdint.h>
4.5.5.2.1 Functions
void CHPMP_Initialize (void)
Initializes the CHPMP module.
void CHPMP_Enable (void)
Enables the CHPMP module.
bool CHPMP_Disable (void)
Disables the CHPMP module. If the return value is False, turn off all analog peripherals and try again.
bool CHPMP_IsVDDAboveVAuto (void)
Returns the status of the CHPMP threshold.
bool CHPMP_IsReady (void)
Returns the status of Steady state.
4.5.5.2.2 Macros
#define myCHPMP_Initialize CHPMP_Initialize
Defines the Custom Name for the CHPMP_Initialize API.
#define myCHPMP_Enable CHPMP_Enable
Defines the Custom Name for the CHPMP_Enable API.
#define myCHPMP_Disable CHPMP_Disable
Defines the Custom Name for the CHPMP_Disable API.
#define myCHPMP_IsVDDAboveVAuto CHPMP_IsVDDAboveVAuto
Defines the Custom Name for the CHPMP_IsVDDAboveVAuto API.
#define myCHPMP_IsReady CHPMP_IsReady
Defines the Custom Name for the CHPMP_IsReady API.
4.5.5.2.3 Detailed Description
CHPMP Generated Driver API Header File