4.27 ZCD - Zero-Crossing Detector
4.27.1 Introduction
The MPLAB® Code Configurator (MCC) Melody Zero-Crossing Detector Peripheral Library (PLIBs) drivers generates APIs to support ZCD-specific peripheral functionality on target MCUs.
The Zero-Crossing Detector (ZCD) module detects when an A/C signal crosses through the ground potential. The actual zero-crossing threshold is the zero-crossing reference voltage, ZCPINV, which is typically 0.75V above ground.
4.27.2 Supported Device Families
| PIC12/16F161x | PIC12/16F184x | PIC16F153xx |
| PIC16F170x | PIC16F171x | PIC16F171xx |
| PIC16F176x | PIC16F177x | PIC16F180xx |
| PIC16F181xx | PIC16F184xx | PIC16F188xx |
| PIC16F191xx | PIC18F-K40 | PIC18F-K42 |
| PIC18F-K83 | PIC18F-Q10 | PIC18F-Q24 |
| PIC18F-Q40 | PIC18F-Q41 | PIC18F-Q43 |
| PIC18F-Q71 | PIC18F-Q83 | PIC18F-Q84 |
4.27.3 Required Header Files:
#include "mcc_generated_files/zcd/zcd.h"
4.27.4 Module Documentation
4.27.4.1 ZCD
This file contains the API prototypes for the ZCD driver.
4.27.4.1.1 Module description
This file contains the API prototypes for the ZCD driver.
Functions
void ZCD_Initialize (void)
Initializes the ZCD module. This is called only once before calling other ZCD APIs.
bool ZCD_IsLogicLevel (void)
Returns the status of the ZCD pin if it is sinking or sourcing current depending on the selected output polarity.
void ZCD_ISR (void)
Implements the Interrupt Service Routine (ISR) for the ZCD interrupt.
4.27.4.1.2 Function Documentation
ZCD_Initialize()
void ZCD_Initialize (void )
Initializes the ZCD module. This is called only once before calling other ZCD APIs.
Section: Included FilesSection: ZCD Module APIs
|
None. |
Section: Included FilesSection: ZCD Module APIs
ZCD_IsLogicLevel()
bool ZCD_IsLogicLevel (void )
Returns the status of the ZCD pin if it is sinking or sourcing current depending on the selected output polarity.
ZCD_Initialize() is already called. |
|
|
ZCD_ISR()
void ZCD_ISR (void )
Implements the Interrupt Service Routine (ISR) for the ZCD interrupt.
|
None. |
4.27.5 File Documentation
4.27.5.1 source/zcd.c File Reference
This file contains the API implementation for the ZCD driver.
#include <xc.h> #include "../zcd.h"
4.27.5.1.1 Functions
void ZCD_Initialize (void)
Initializes the ZCD module. This is called only once before calling other ZCD APIs.
bool ZCD_IsLogicLevel (void)
Returns the status of the ZCD pin if it is sinking or sourcing current depending on the selected output polarity.
void ZCD_ISR (void)
Implements the Interrupt Service Routine (ISR) for the ZCD interrupt.
4.27.5.1.2 Detailed Description
This file contains the API implementation for the ZCD driver.
ZCD Generated Driver File.
4.27.5.2 source/zcd.h File Reference
#include <xc.h> #include <stdbool.h> #include <stdint.h>
4.27.5.2.1 Functions
void ZCD_Initialize (void)
Initializes the ZCD module. This is called only once before calling other ZCD APIs.
bool ZCD_IsLogicLevel (void)
Returns the status of the ZCD pin if it is sinking or sourcing current depending on the selected output polarity.
void ZCD_ISR (void)
Implements the Interrupt Service Routine (ISR) for the ZCD interrupt.
4.27.5.2.2 Detailed Description
ZCD Generated Driver API Header File.