4.24.3.2 TMR2 with One-Shot Operation
Timer2 with One-Shot Operation
4.24.3.2.1 Introduction
The Timer2 (TMR2) module is a 8-bit timer that operates by a matching the value written to a configurable 8-bit period register.
4.24.3.2.2 Supported Device Families
| PIC12/16F161x | PIC16F152xx | PIC16F153xx |
| PIC16F171x | PIC16F171xx | PIC16F176x |
| PIC16F177x | PIC16F180xx | PIC16F181xx |
| PIC16F184x | PIC16F184xx | PIC16F188xx |
| PIC16F191xx | PIC18F-K40 | PIC18F-K42 |
| PIC18F-K83 | PIC18F-Q10 | PIC18F-Q20 |
| PIC18F-Q40 | PIC18F-Q41 | PIC18F-Q43 |
| PIC18F-Q71 | PIC18F-Q83 | PIC18F-Q84 |
4.24.3.2.3 Required header files:
#include "mcc_generated_files/timer/tmr2.h"
4.24.3.2.4 How to use the Timer 2 PLIB
Click the links to view the code snippets associated with each example:
- Timer2 Use Case 1: Timer Period Change This example demonstrates an application where the timer period changes from 4 ms to 8 ms and vice versa with every overflow of the timer.
- Timer2 Use Case 2: LED Toggle at Overflow This example toggles an LED when an overflow interrupt event occurs.
- Timer2 Use Case 3: Timer Wake from Sleep at Interrupt event This example wakes the microcontroller from Sleep mode every five seconds.
4.24.3.2.5 Specific MISRA C:2012 Deviations
- Global TMR2_MAX_COUNT
-
Advisory: misra-c2012-2.5
Justification: MCC Melody drivers provide macros that can be added to an application. It depends on the application whether a macro is used or not.Advisory: misra-c2012-2.5
Justification: MCC Melody drivers provide macros that can be added to an application. It depends on the application whether a macro is used or not. - Global TMR2_Read
-
Advisory: misra-c2012-2.5
Justification: MCC Melody drivers provide macros that can be added to an application. It depends on the application whether a macro is used or not.
4.24.3.2.6 Module Documentation
TMR2
This file contains API prototypes and other data types for the TMR2 driver.
Module description
This file contains API prototypes and other data types for the TMR2 driver.
This file contains deprecated macros or functions for the TMR2 driver.
Definitions
#define TMR2_MAX_COUNT (255U)
Defines the TMR2 maximum count value.
#define TMR2_CLOCK_FREQ (16000000UL)
Defines the TMR2 prescaled clock frequency in hertz.
#define TIMER2_MAX_COUNT TMR2_MAX_COUNT
Defines the Custom Name for the TMR2_MAX_COUNT.
#define TIMER2_CLOCK_FREQ TMR2_CLOCK_FREQ
Defines the Custom Name for the TMR2_CLOCK_FREQ.
#define Timer2_Initialize TMR2_Initialize
Defines the Custom Name for the TMR2_Initialize API.
#define Timer2_Deinitialize TMR2_Deinitialize
Defines the Custom Name for the TMR2_Deinitialize API.
#define Timer2_Start TMR2_Start
Defines the Custom Name for the TMR2_Start API.
#define Timer2_Stop TMR2_Stop
Defines the Custom Name for the TMR2_Stop API.
#define Timer2_CounterGet TMR2_CounterGet
Defines the Custom Name for the TMR2_CounterGet API.
#define Timer2_CounterSet TMR2_CounterSet
Defines the Custom Name for the TMR2_CounterSet API.
#define Timer2_PeriodSet TMR2_PeriodSet
Defines the Custom Name for the TMR2_PeriodSet API.
#define Timer2_MaxCountGet TMR2_MaxCountGet
Defines the Custom Name for the TMR2_MaxCountGet API.
#define Timer2_ModeSet TMR2_ModeSet
Defines the Custom Name for the TMR2_ModeSet API.
#define Timer2_ExtResetSourceSet TMR2_ExtResetSourceSet
Defines the Custom Name for the TMR2_ExtResetSourceSet API.
#define Timer2_PeriodMatchCallbackRegister TMR2_PeriodMatchCallbackRegister
Defines the Custom Name for the TMR2_PeriodMatchCallbackRegister API.
#define Timer2_PeriodMatchStatusGet TMR2_PeriodMatchStatusGet
Defines the Custom Name for the TMR2_PeriodMatchStatusGet API.
#define Timer2_PeriodMatchStatusClear TMR2_PeriodMatchStatusClear
Defines the Custom Name for the TMR2_PeriodMatchStatusClear API.
#define Timer2_TMRInterruptEnable TMR2_TMRInterruptEnable
Defines the Custom Name for the TMR2_TMRInterruptEnable API.
#define Timer2_TMRInterruptDisable TMR2_TMRInterruptDisable
Defines the Custom Name for the TMR2_TMRInterruptDisable API.
#define Timer2_ISR TMR2_ISR
Defines the Custom Name for the TMR2_ISR API.
#define Timer2_Tasks TMR2_Tasks
Defines the Custom Name for the TMR2_Tasks API.
#define TMR2_Read TMR2_CounterGet
Defines the Custom Name for the TMR2_CounterGet API. The TMR2_Read will be deprecated in the future release. Use TMR2_CounterGet instead.
#define Timer2_Read TMR2_CounterGet
Defines the Custom Name for the TMR2_CounterGet API. The Timer2_Read will be deprecated in the future release. Use Timer2_CounterGet instead.
#define TMR2_Write TMR2_CounterSet
Defines the Custom Name for the TMR2_CounterSet API. The TMR2_Write will be deprecated in the future release. Use TMR2_CounterSet instead.
#define Timer2_Write TMR2_CounterSet
Defines the Custom Name for the TMR2_CounterSet API. The Timer2_Write will be deprecated in the future release. Use Timer2_CounterSet instead.
#define TMR2_PeriodCountSet TMR2_PeriodSet
Defines the Custom Name for the TMR2_PeriodSet API. The TMR2_PeriodCountSet will be deprecated in the future release. Use TMR2_PeriodSet instead.
#define Timer2_PeriodCountSet TMR2_PeriodSet
Defines the Custom Name for the TMR2_PeriodSet API. The Timer2_PeriodCountSet will be deprecated in the future release. Use Timer2_PeriodSet instead.
#define TMR2_OverflowCallbackRegister TMR2_PeriodMatchCallbackRegister
Defines the Custom Name for the TMR2_PeriodMatchCallbackRegister API. The TMR2_OverflowCallbackRegister will be deprecated in the future release. Use TMR2_PeriodMatchCallbackRegister instead.
#define Timer2_OverflowCallbackRegister TMR2_PeriodMatchCallbackRegister
Defines the Custom Name for the TMR2_PeriodMatchCallbackRegister API. The Timer2_OverflowCallbackRegister will be deprecated in the future release. Use Timer2_PeriodMatchCallbackRegister instead.
Enumerations
enum TMR2_HLT_EXT_RESET_SOURCE { TMR2_T2CKIPPS_PIN = 0x0, TMR2_TMR4_POSTSCALED = 0x2, TMR2_TMR6_POSTSCALED = 0x3, TMR2_CCP1OUT = 0x4, TMR2_CCP2OUT = 0x5, TMR2_CCP3OUT = 0x6, TMR2_PWM1_OUT1 = 0x7, TMR2_PWM1_OUT2 = 0x8, TMR2_PWM2_OUT1 = 0x9, TMR2_PWM2_OUT2 = 0xa, TMR2_PWM3_OUT1 = 0xb, TMR2_PWM3_OUT2 = 0xc, TMR2_PWM4_OUT1 = 0xd, TMR2_PWM4_OUT2 = 0xe, TMR2_CMP1OUT = 0xf, TMR2_CMP2OUT = 0x10, TMR2_ZCDOUT = 0x11, TMR2_CLC1_OUT = 0x12, TMR2_CLC2_OUT = 0x13, TMR2_CLC3_OUT = 0x14, TMR2_CLC4_OUT = 0x15, TMR2_CLC5_OUT = 0x16, TMR2_CLC6_OUT = 0x17, TMR2_CLC7_OUT = 0x18, TMR2_CLC8_OUT = 0x19, TMR2_UART1_RX_EDGE = 0x1a, TMR2_UART1_TX_EDGE = 0x1b, TMR2_UART2_RX_EDGE = 0x1c, TMR2_UART2_TX_EDGE = 0x1d, TMR2_UART3_RX_EDGE = 0x1e, TMR2_UART3_TX_EDGE = 0x1f, TMR2_UART4_RX_EDGE = 0x20, TMR2_UART4_TX_EDGE = 0x21, TMR2_UART5_RX_EDGE = 0x22, TMR2_UART5_TX_EDGE = 0x23 }
Defines the several modes of operation of the timer with the HLT extension.
Functions
void TMR2_Initialize (void)
Initializes the Timer2 (TMR2) module. This routine must be called before any other TMR2 routines.
void TMR2_Deinitialize (void)
Deinitializes the TMR2 to POR values.
void TMR2_Start (void)
Starts the TMR2 timer.
void TMR2_Stop (void)
Stops the TMR2 timer.
uint8_t TMR2_CounterGet (void)
Returns the current counter value.
void TMR2_CounterSet (uint8_t count)
Sets the counter value for the TMR2 timer.
void TMR2_PeriodSet (uint8_t periodVal)
Sets the period count value.
uint8_t TMR2_PeriodGet (void)
Returns the current period count value.
uint8_t TMR2_MaxCountGet (void)
Returns the TMR2 maximum count value.
void TMR2_ModeSet (TMR2_HLT_MODE mode)
Sets the Hardware Limit Timer (HLT) mode.
void TMR2_ExtResetSourceSet (TMR2_HLT_EXT_RESET_SOURCE reset)
Sets the HLT External Reset source.
bool TMR2_PeriodMatchStatusGet (void)
Returns the status of the TMR2 Period Match Interrupt flag.
void TMR2_PeriodMatchStatusClear (void)
Clears the TMR2 Period Match Interrupt flag.
void TMR2_Tasks (void)
Performs tasks to be executed during the TMR2 period match event.
void TMR2_TMRInterruptEnable (void)
Enables the TMR2 interrupt.
void TMR2_TMRInterruptDisable (void)
Disables the TMR2 interrupt.
void TMR2_ISR (void)
Interrupt Service Routine (ISR) for the TMR2 period match interrupt.
void TMR2_PeriodMatchCallbackRegister (void(*callbackHandler)(void))
Setter function for the TMR2 period match event.
Definition Documentation
TIMER2_CLOCK_FREQ
#define TIMER2_CLOCK_FREQ TMR2_CLOCK_FREQ
Defines the Custom Name for the TMR2_CLOCK_FREQ.
Timer2_CounterGet
#define Timer2_CounterGet TMR2_CounterGet
Defines the Custom Name for the TMR2_CounterGet API.
Timer2_CounterSet
#define Timer2_CounterSet TMR2_CounterSet
Defines the Custom Name for the TMR2_CounterSet API.
Timer2_Deinitialize
#define Timer2_Deinitialize TMR2_Deinitialize
Defines the Custom Name for the TMR2_Deinitialize API.
Timer2_ExtResetSourceSet
#define Timer2_ExtResetSourceSet TMR2_ExtResetSourceSet
Defines the Custom Name for the TMR2_ExtResetSourceSet API.
Timer2_Initialize
#define Timer2_Initialize TMR2_Initialize
Defines the Custom Name for the TMR2_Initialize API.
Timer2_ISR
#define Timer2_ISR TMR2_ISR
Defines the Custom Name for the TMR2_ISR API.
TIMER2_MAX_COUNT
#define TIMER2_MAX_COUNT TMR2_MAX_COUNT
Defines the Custom Name for the TMR2_MAX_COUNT.
Timer2_MaxCountGet
#define Timer2_MaxCountGet TMR2_MaxCountGet
Defines the Custom Name for the TMR2_MaxCountGet API.
Timer2_ModeSet
#define Timer2_ModeSet TMR2_ModeSet
Defines the Custom Name for the TMR2_ModeSet API.
Timer2_OverflowCallbackRegister
#define Timer2_OverflowCallbackRegister TMR2_PeriodMatchCallbackRegister
Defines the Custom Name for the TMR2_PeriodMatchCallbackRegister API. The Timer2_OverflowCallbackRegister will be deprecated in the future release. Use Timer2_PeriodMatchCallbackRegister instead.
Timer2_PeriodCountSet
#define Timer2_PeriodCountSet TMR2_PeriodSet
Defines the Custom Name for the TMR2_PeriodSet API. The Timer2_PeriodCountSet will be deprecated in the future release. Use Timer2_PeriodSet instead.
Timer2_PeriodGet
#define Timer2_PeriodGet TMR2_PeriodGet
Defines the Custom Name for the TMR2_PeriodGet API.
Timer2_PeriodMatchCallbackRegister
#define Timer2_PeriodMatchCallbackRegister TMR2_PeriodMatchCallbackRegister
Defines the Custom Name for the TMR2_PeriodMatchCallbackRegister API.
Timer2_PeriodMatchStatusClear
#define Timer2_PeriodMatchStatusClear TMR2_PeriodMatchStatusClear
Defines the Custom Name for the TMR2_PeriodMatchStatusClear API.
Timer2_PeriodMatchStatusGet
#define Timer2_PeriodMatchStatusGet TMR2_PeriodMatchStatusGet
Defines the Custom Name for the TMR2_PeriodMatchStatusGet API.
Timer2_PeriodSet
#define Timer2_PeriodSet TMR2_PeriodSet
Defines the Custom Name for the TMR2_PeriodSet API.
Timer2_Read
#define Timer2_Read TMR2_CounterGet
Defines the Custom Name for the TMR2_CounterGet API. The Timer2_Read will be deprecated in the future release. Use Timer2_CounterGet instead.
Timer2_Start
#define Timer2_Start TMR2_Start
Defines the Custom Name for the TMR2_Start API.
Timer2_Stop
#define Timer2_Stop TMR2_Stop
Defines the Custom Name for the TMR2_Stop API.
Timer2_Tasks
#define Timer2_Tasks TMR2_Tasks
Defines the Custom Name for the TMR2_Tasks API.
Timer2_TMRInterruptDisable
#define Timer2_TMRInterruptDisable TMR2_TMRInterruptDisable
Defines the Custom Name for the TMR2_TMRInterruptDisable API.
Timer2_TMRInterruptEnable
#define Timer2_TMRInterruptEnable TMR2_TMRInterruptEnable
Defines the Custom Name for the TMR2_TMRInterruptEnable API.
Timer2_Write
#define Timer2_Write TMR2_CounterSet
Defines the Custom Name for the TMR2_CounterSet API. The Timer2_Write will be deprecated in the future release. Use Timer2_CounterSet instead.
TMR2_CLOCK_FREQ
#define TMR2_CLOCK_FREQ (16000000UL)
Defines the TMR2 prescaled clock frequency in hertz.
TMR2_MAX_COUNT
#define TMR2_MAX_COUNT (255U)
Defines the TMR2 maximum count value.
MISRA C:2012 Deviation Advisory: misra-c2012-2.5
Justification: MCC Melody drivers provide macros that can be added to an application. It depends on the application whether a macro is used or not.TMR2_OverflowCallbackRegister
#define TMR2_OverflowCallbackRegister TMR2_PeriodMatchCallbackRegister
Defines the Custom Name for the TMR2_PeriodMatchCallbackRegister API. The TMR2_OverflowCallbackRegister will be deprecated in the future release. Use TMR2_PeriodMatchCallbackRegister instead.
TMR2_PeriodCountSet
#define TMR2_PeriodCountSet TMR2_PeriodSet
Defines the Custom Name for the TMR2_PeriodSet API. The TMR2_PeriodCountSet will be deprecated in the future release. Use TMR2_PeriodSet instead.
TMR2_Read
#define TMR2_Read TMR2_CounterGet
Defines the Custom Name for the TMR2_CounterGet API. The TMR2_Read will be deprecated in the future release. Use TMR2_CounterGet instead.
MISRA C:2012 Deviation Advisory: misra-c2012-2.5
Justification: MCC Melody drivers provide macros that can be added to an application. It depends on the application whether a macro is used or not.TMR2_Write
#define TMR2_Write TMR2_CounterSet
Defines the Custom Name for the TMR2_CounterSet API. The TMR2_Write will be deprecated in the future release. Use TMR2_CounterSet instead.
Function Documentation
TMR2_CounterGet()
uint8_t TMR2_CounterGet (void )
Returns the current counter value.
Initialize TMR2 with TMR2_Initialize() before calling this API. |
| None. |
Current counter value |
TMR2_CounterSet()
void TMR2_CounterSet (uint8_t count)
Sets the counter value for the TMR2 timer.
Initialize TMR2 with TMR2_Initialize() before calling this API. |
| count |
- Counter value to be written to the T2TMR register |
None. |
TMR2_Deinitialize()
void TMR2_Deinitialize (void )
Deinitializes the TMR2 to POR values.
| None. |
None. |
TMR2_ExtResetSourceSet()
void TMR2_ExtResetSourceSet (TMR2_HLT_EXT_RESET_SOURCE reset)
Sets the HLT External Reset source.
Initialize TMR2 with TMR2_Initialize() before calling this API. |
| reset |
- Value to be written to the T2RSTbits.RSEL bits |
None. |
TMR2_Initialize()
void TMR2_Initialize (void )
Initializes the Timer2 (TMR2) module. This routine must be called before any other TMR2 routines.
Section: TMR2 APIs
| None. |
None. |
Section: TMR2 APIs
TMR2_ISR()
void TMR2_ISR (void )
Interrupt Service Routine (ISR) for the TMR2 period match interrupt.
| None. |
None. |
TMR2_MaxCountGet()
uint8_t TMR2_MaxCountGet (void )
Returns the TMR2 maximum count value.
| None. |
Maximum count value |
TMR2_ModeSet()
void TMR2_ModeSet (TMR2_HLT_MODE mode)
Sets the Hardware Limit Timer (HLT) mode.
Initialize TMR2 with TMR2_Initialize() after calling this API. |
| mode |
- Value to be written to the T2HLTbits.MODE bits |
None. |
TMR2_PeriodGet()
uint8_t TMR2_PeriodGet (void )
Returns the current period count value.
Initialize TMR2 with TMR2_Initialize() before calling this API. |
| None. |
Period count value from the T2PR register |
TMR2_PeriodMatchCallbackRegister()
void TMR2_PeriodMatchCallbackRegister (void(*)(void) callbackHandler)
Setter function for the TMR2 period match event.
| CallbackHandler |
- Address of the custom callback function |
None. |
TMR2_PeriodMatchStatusClear()
void TMR2_PeriodMatchStatusClear (void )
Clears the TMR2 Period Match Interrupt flag.
| None. |
None. |
TMR2_PeriodMatchStatusGet()
bool TMR2_PeriodMatchStatusGet (void )
Returns the status of the TMR2 Period Match Interrupt flag.
| None. |
Interrupt flag status |
TMR2_PeriodSet()
void TMR2_PeriodSet (uint8_t periodVal)
Sets the period count value.
Initialize TMR2 with TMR2_Initialize() before calling this API. |
| periodVal |
- Period count value to be written to the T2PR register |
None. |
TMR2_Start()
void TMR2_Start (void )
Starts the TMR2 timer.
Initialize TMR2 with TMR2_Initialize() before calling this API. |
| None. |
None. |
TMR2_Stop()
void TMR2_Stop (void )
Stops the TMR2 timer.
Initialize TMR2 with TMR2_Initialize() before calling this API. |
| None. |
None. |
TMR2_Tasks()
void TMR2_Tasks (void )
Performs tasks to be executed during the TMR2 period match event.
| None. |
None. |
TMR2_TMRInterruptDisable()
void TMR2_TMRInterruptDisable (void )
Disables the TMR2 interrupt.
| None. |
None. |
TMR2_TMRInterruptEnable()
void TMR2_TMRInterruptEnable (void )
Enables the TMR2 interrupt.
| None. |
None. |
Enumeration Type Documentation
TMR2_HLT_EXT_RESET_SOURCE
enum TMR2_HLT_EXT_RESET_SOURCE
Defines the several modes of operation of the timer with the HLT extension.
Defines the different Reset sources of the HLT.
| TMR2_T2CKIPPS_PIN | |
| TMR2_TMR4_POSTSCALED | |
| TMR2_TMR6_POSTSCALED | |
| TMR2_CCP1OUT | |
| TMR2_CCP2OUT | |
| TMR2_CCP3OUT | |
| TMR2_PWM1_OUT1 | |
| TMR2_PWM1_OUT2 | |
| TMR2_PWM2_OUT1 | |
| TMR2_PWM2_OUT2 | |
| TMR2_PWM3_OUT1 | |
| TMR2_PWM3_OUT2 | |
| TMR2_PWM4_OUT1 | |
| TMR2_PWM4_OUT2 | |
| TMR2_CMP1OUT | |
| TMR2_CMP2OUT | |
| TMR2_ZCDOUT | |
| TMR2_CLC1_OUT | |
| TMR2_CLC2_OUT | |
| TMR2_CLC3_OUT | |
| TMR2_CLC4_OUT | |
| TMR2_CLC5_OUT | |
| TMR2_CLC6_OUT | |
| TMR2_CLC7_OUT | |
| TMR2_CLC8_OUT | |
| TMR2_UART1_RX_EDGE | |
| TMR2_UART1_TX_EDGE | |
| TMR2_UART2_RX_EDGE | |
| TMR2_UART2_TX_EDGE | |
| TMR2_UART3_RX_EDGE | |
| TMR2_UART3_TX_EDGE | |
| TMR2_UART4_RX_EDGE | |
| TMR2_UART4_TX_EDGE | |
| TMR2_UART5_RX_EDGE | |
| TMR2_UART5_TX_EDGE |
4.24.3.2.7 TMR2 Examples
This section explains various use case examples of the Timer module within an MPLAB® Code Configurator (MCC) Melody Project.
TMR2 PLIB Examples
4 ms/8 ms Timer Period Change in Non-Interrupt Mode
This use case configures the TMR2 PLIB to generate the timer period. The period of a timer is changed at run time during each overflow event. The callback function is used to change the timer period.
-
System>Clock Control:
-
Clock Source: HFINTOSC
-
HF Internal Clock: 64 MHz
-
-
System>Pins:
-
Pin Grid View: Select LED pin as output (Check the schematic for your board)
-
Pins: Rename Custom Name to "LED"
-
-
Drivers>TMR2:
-
Timer Enable: False
-
Prescaler: 1:128
-
Postscaler: 1:16
-
TMR Interrupt Enable: False
-
After configuring the components as described above, click 'Generate' to generate the code. Then add the following code snippets to your application:
#include "mcc_generated_files/system/system.h" /* * Development Board: PIC18F57Q43 Curiosity Nano Board * MCC Configuration: * System module: HFINTOSC (64 MHz) * TMR2 module: Timer Enable - False, Prescaler - 1:128, Postscaler - 1:16, TMR Interrupt Enable - False * Pins module: RF3 - GPIO Output, CustomName - LED */ #define USE_TASKS_API 1 #define POSTSCALER 16UL #define MS_TO_TICKS(ms) (((TMR2_CLOCK_FREQ * (ms)) / 1000UL) - 1UL) #define LED_4_MS (MS_TO_TICKS(4UL)/POSTSCALER) #define LED_8_MS (MS_TO_TICKS(8UL)/POSTSCALER) static void Timer_PeriodChange(void) { static volatile bool changePeriod = false; LED_Toggle(); TMR2_Stop(); uint8_t maxCount = TMR2_MaxCountGet(); uint8_t newPeriod = changePeriod ? LED_4_MS:LED_8_MS; if(maxCount > newPeriod) { TMR2_PeriodSet(newPeriod); } else { // Invalid period } changePeriod = !changePeriod; TMR2_Start(); } int main(void) { SYSTEM_Initialize(); TMR2_PeriodSet(LED_4_MS); TMR2_PeriodMatchStatusClear(); #if USE_TASKS_API TMR2_PeriodMatchCallbackRegister(Timer_PeriodChange); #endif TMR2_Start(); while(1) { #if USE_TASKS_API TMR2_Tasks(); #else if(1U == TMR2_PeriodMatchStatusGet()) { Timer_PeriodChange(); TMR2_PeriodMatchStatusClear(); } #endif } }
4 ms Timer Period in Interrupt Mode
This use case configures the TMR2 PLIB to generate the overflow interrupt at a period of 4 ms, while toggling an LED. This use case uses the generated APIs to set the timer period.
-
System>Clock Control:
-
Clock Source: HFINTOSC
-
HF Internal Clock: 64 MHz
-
-
System>Pins:
-
Pin Grid View: Select LED pin as output (Check the schematic for your board)
-
Pins: Rename Custom Name to "LED"
-
-
Drivers>TMR2:
-
Timer Enable: False
-
Clock Source: FOSC/4
-
Prescaler: 1:64
-
Postscaler: 1:8
-
TMR Interrupt Enable: True
-
After configuring the components as described above, click 'Generate' to generate the code. Then add the following code snippets to your application:
#include "mcc_generated_files/system/system.h" /* * Development Board: PIC18F57Q43 Curiosity Nano Board * MCC Configuration: * System module: HFINTOSC (64 MHz) * TMR2 module: Timer Enable - False, Clock Source - FOSC/4, Prescaler - 1:64, Postscaler - 1:8, TMR Interrupt Enable - True * Pins module: RF3 - GPIO Output, CustomName - LED */ #define POSTSCALER 8UL #define MS_TO_TICKS(ms) (((TMR2_CLOCK_FREQ * (ms)) / 1000UL) - 1UL) #define LED_4_MS (MS_TO_TICKS(4UL)/POSTSCALER) void Custom_Callback(void) { LED_Toggle(); } int main(void) { SYSTEM_Initialize(); const uint8_t maxCount = TMR2_MaxCountGet(); TMR2_CounterSet(0); if(maxCount > LED_4_MS) { TMR2_PeriodSet(LED_4_MS); } else { // Invalid period // Generate default timer period } TMR2_PeriodMatchCallbackRegister(Custom_Callback); TMR2_Start(); INTERRUPT_GlobalInterruptEnable(); while(1) { } }
Timer Wake From Sleep At Every 5s
This use case configures the TMR2 PLIB to wake the microcontroller (MCU) from Sleep mode every five seconds. The wake up event toggles an LED, then puts the MCU back to Sleep.
-
System>Clock Control:
-
Clock Source: HFINTOSC
-
HF Internal Clock: 64 MHz
-
-
System>Pins:
-
Pin Grid View: Select LED pin as output (Check the schematic for your board)
-
Pins: Rename Custom Name to "LED"
-
-
Drivers>TMR2:
-
Timer Enable: True
-
Clock Source: LFINTOSC
-
Prescaler: 1:64
-
Postscaler: 1:16
-
Requested Period: 5s
-
TMR Interrupt Enable: True
-
After configuring the components as described above, click 'Generate' to generate the code. Then add the following code snippets to your application:
#include "mcc_generated_files/system/system.h" /* * Development Board: PIC18F57Q43 Curiosity Nano Board * MCC Configuration: * System module: HFINTOSC (64 MHz) * TMR2 module: Timer Enable - True, Clock Source - LFINTOSC, Synchronization Enable - False, Prescaler - 1:64, Postscaler - 1:16, Requested Period - 5s, TMR Interrupt Enable - True * Pins module: RF3 - GPIO Output, CustomName - LED */ int main(void) { SYSTEM_Initialize(); // Enable the Global Interrupts INTERRUPT_GlobalInterruptEnable(); while(1) { LED_Toggle(); SLEEP(); // Add your code here to execute after exiting Sleep mode } }
4.24.3.2.8 File Documentation
source/tmr2.c File Reference
Driver implementation for the TMR2 module.
#include <xc.h> #include "../tmr2.h"
Functions
static void TMR2_DefaultPeriodMatchCallback (void)
void TMR2_Initialize (void)
Initializes the Timer2 (TMR2) module. This routine must be called before any other TMR2 routines.
void TMR2_Deinitialize (void)
Deinitializes the TMR2 to POR values.
void TMR2_Start (void)
Starts the TMR2 timer.
void TMR2_Stop (void)
Stops the TMR2 timer.
void TMR2_ModeSet (TMR2_HLT_MODE mode)
Sets the Hardware Limit Timer (HLT) mode.
void TMR2_ExtResetSourceSet (TMR2_HLT_EXT_RESET_SOURCE reset)
Sets the HLT External Reset source.
uint8_t TMR2_CounterGet (void)
Returns the current counter value.
void TMR2_CounterSet (uint8_t count)
Sets the counter value for the TMR2 timer.
void TMR2_PeriodSet (uint8_t periodVal)
Sets the period count value.
uint8_t TMR2_PeriodGet (void)
Returns the current period count value.
uint8_t TMR2_MaxCountGet (void)
Returns the TMR2 maximum count value.
bool TMR2_PeriodMatchStatusGet (void)
Returns the status of the TMR2 Period Match Interrupt flag.
void TMR2_PeriodMatchStatusClear (void)
Clears the TMR2 Period Match Interrupt flag.
void TMR2_Tasks (void)
Performs tasks to be executed during the TMR2 period match event.
void TMR2_PeriodMatchCallbackRegister (void(*callbackHandler)(void))
Setter function for the TMR2 period match event.
Variables
static void(* TMR2_PeriodMatchCallback )(void)
Detailed Description
Driver implementation for the TMR2 module.
Driver implementation for the TMR2 Timer driver.
TMR2 Generated Driver File
TMR2 Generated Timer Driver File
Function Documentation
TMR2_DefaultPeriodMatchCallback()
static void TMR2_DefaultPeriodMatchCallback (void )[static]
Variable Documentation
TMR2_PeriodMatchCallback
void(* TMR2_PeriodMatchCallback) (void)[static]
Section: Included Files
source/tmr2.h File Reference
This file contains API prototypes and other data types for the TMR2 Timer driver.
#include <stdint.h> #include <stdbool.h> #include "tmr2_deprecated.h"
Functions
void TMR2_Initialize (void)
Initializes the Timer2 (TMR2) module. This routine must be called before any other TMR2 routines.
void TMR2_Deinitialize (void)
Deinitializes the TMR2 to POR values.
void TMR2_Start (void)
Starts the TMR2 timer.
void TMR2_Stop (void)
Stops the TMR2 timer.
uint8_t TMR2_CounterGet (void)
Returns the current counter value.
void TMR2_CounterSet (uint8_t count)
Sets the counter value for the TMR2 timer.
void TMR2_PeriodSet (uint8_t periodVal)
Sets the period count value.
uint8_t TMR2_PeriodGet (void)
Returns the current period count value.
uint8_t TMR2_MaxCountGet (void)
Returns the TMR2 maximum count value.
void TMR2_ModeSet (TMR2_HLT_MODE mode)
Sets the Hardware Limit Timer (HLT) mode.
void TMR2_ExtResetSourceSet (TMR2_HLT_EXT_RESET_SOURCE reset)
Sets the HLT External Reset source.
bool TMR2_PeriodMatchStatusGet (void)
Returns the status of the TMR2 Period Match Interrupt flag.
void TMR2_PeriodMatchStatusClear (void)
Clears the TMR2 Period Match Interrupt flag.
void TMR2_Tasks (void)
Performs tasks to be executed during the TMR2 period match event.
void TMR2_TMRInterruptEnable (void)
Enables the TMR2 interrupt.
void TMR2_TMRInterruptDisable (void)
Disables the TMR2 interrupt.
void TMR2_ISR (void)
Interrupt Service Routine (ISR) for the TMR2 period match interrupt.
void TMR2_PeriodMatchCallbackRegister (void(*callbackHandler)(void))
Setter function for the TMR2 period match event.
Macros
-
#define TMR2_MAX_COUNT (255U)
Defines the TMR2 maximum count value.
-
#define TMR2_CLOCK_FREQ (16000000UL)
Defines the TMR2 prescaled clock frequency in hertz.
-
#define TIMER2_MAX_COUNT TMR2_MAX_COUNT
Defines the Custom Name for the TMR2_MAX_COUNT.
-
#define TIMER2_CLOCK_FREQ TMR2_CLOCK_FREQ
Defines the Custom Name for the TMR2_CLOCK_FREQ.
-
#define Timer2_Initialize TMR2_Initialize
Defines the Custom Name for the TMR2_Initialize API.
-
#define Timer2_Deinitialize TMR2_Deinitialize
Defines the Custom Name for the TMR2_Deinitialize API.
-
#define Timer2_Start TMR2_Start
Defines the Custom Name for the TMR2_Start API.
-
#define Timer2_Stop TMR2_Stop
Defines the Custom Name for the TMR2_Stop API.
-
#define Timer2_CounterGet TMR2_CounterGet
Defines the Custom Name for the TMR2_CounterGet API.
-
#define Timer2_CounterSet TMR2_CounterSet
Defines the Custom Name for the TMR2_CounterSet API.
-
#define Timer2_PeriodSet TMR2_PeriodSet
Defines the Custom Name for the TMR2_PeriodSet API.
-
#define Timer2_MaxCountGet TMR2_MaxCountGet
Defines the Custom Name for the TMR2_MaxCountGet API.
-
#define Timer2_ModeSet TMR2_ModeSet
Defines the Custom Name for the TMR2_ModeSet API.
-
#define Timer2_ExtResetSourceSet TMR2_ExtResetSourceSet
Defines the Custom Name for the TMR2_ExtResetSourceSet API.
-
#define Timer2_PeriodMatchCallbackRegister TMR2_PeriodMatchCallbackRegister
Defines the Custom Name for the TMR2_PeriodMatchCallbackRegister API.
-
#define Timer2_PeriodMatchStatusGet TMR2_PeriodMatchStatusGet
Defines the Custom Name for the TMR2_PeriodMatchStatusGet API.
-
#define Timer2_PeriodMatchStatusClear TMR2_PeriodMatchStatusClear
Defines the Custom Name for the TMR2_PeriodMatchStatusClear API.
-
#define Timer2_TMRInterruptEnable TMR2_TMRInterruptEnable
Defines the Custom Name for the TMR2_TMRInterruptEnable API.
-
#define Timer2_TMRInterruptDisable TMR2_TMRInterruptDisable
Defines the Custom Name for the TMR2_TMRInterruptDisable API.
-
#define Timer2_ISR TMR2_ISR
Defines the Custom Name for the TMR2_ISR API.
-
#define Timer2_Tasks TMR2_Tasks
Defines the Custom Name for the TMR2_Tasks API.
Enumerations
enum TMR2_HLT_MODE { TMR2_ROP_STARTS_TMRON, TMR2_ROP_STARTS_TMRON_ERSHIGH, TMR2_ROP_STARTS_TMRON_ERSLOW, TMR2_ROP_RESETS_ERSBOTHEDGE, TMR2_ROP_RESETS_ERSRISINGEDGE, TMR2_ROP_RESETS_ERSFALLINGEDGE, TMR2_ROP_RESETS_ERSLOW, TMR2_ROP_RESETS_ERSHIGH, TMR2_OS_STARTS_TMRON, TMR2_OS_STARTS_ERSRISINGEDGE, TMR2_OS_STARTS_ERSFALLINGEDGE, TMR2_OS_STARTS_ERSBOTHEDGE, TMR2_OS_STARTS_ERSFIRSTRISINGEDGE, TMR2_OS_STARTS_ERSFIRSTFALLINGEDGE, TMR2_OS_STARTS_ERSRISINGEDGEDETECT, TMR2_OS_STARTS_ERSFALLINGEDGEDETECT, TMR2_OS_STARTS_TMRON_ERSHIGH = 0x16, TMR2_OS_STARTS_TMRON_ERSLOW = 0x17, TMR2_MS_STARTS_TMRON_ERSRISINGEDGEDETECT = 0x11, TMR2_MS_STARTS_TMRON_ERSFALLINGEDGEDETECT = 0x12, TMR2_MS_STARTS_TMRON_ERSBOTHEDGE = 0x13 }
enum TMR2_HLT_EXT_RESET_SOURCE { TMR2_T2CKIPPS_PIN = 0x0, TMR2_TMR4_POSTSCALED = 0x2, TMR2_TMR6_POSTSCALED = 0x3, TMR2_CCP1OUT = 0x4, TMR2_CCP2OUT = 0x5, TMR2_CCP3OUT = 0x6, TMR2_PWM1_OUT1 = 0x7, TMR2_PWM1_OUT2 = 0x8, TMR2_PWM2_OUT1 = 0x9, TMR2_PWM2_OUT2 = 0xa, TMR2_PWM3_OUT1 = 0xb, TMR2_PWM3_OUT2 = 0xc, TMR2_PWM4_OUT1 = 0xd, TMR2_PWM4_OUT2 = 0xe, TMR2_CMP1OUT = 0xf, TMR2_CMP2OUT = 0x10, TMR2_ZCDOUT = 0x11, TMR2_CLC1_OUT = 0x12, TMR2_CLC2_OUT = 0x13, TMR2_CLC3_OUT = 0x14, TMR2_CLC4_OUT = 0x15, TMR2_CLC5_OUT = 0x16, TMR2_CLC6_OUT = 0x17, TMR2_CLC7_OUT = 0x18, TMR2_CLC8_OUT = 0x19, TMR2_UART1_RX_EDGE = 0x1a, TMR2_UART1_TX_EDGE = 0x1b, TMR2_UART2_RX_EDGE = 0x1c, TMR2_UART2_TX_EDGE = 0x1d, TMR2_UART3_RX_EDGE = 0x1e, TMR2_UART3_TX_EDGE = 0x1f, TMR2_UART4_RX_EDGE = 0x20, TMR2_UART4_TX_EDGE = 0x21, TMR2_UART5_RX_EDGE = 0x22, TMR2_UART5_TX_EDGE = 0x23 }
Defines the several modes of operation of the timer with the HLT extension.
Detailed Description
This file contains API prototypes and other data types for the TMR2 Timer driver.
TMR2 Generated Driver API Header File
TMR2 Generated Timer Driver API Header File
Enumeration Type Documentation
TMR2_HLT_MODE
enum TMR2_HLT_MODE
| TMR2_ROP_STARTS_TMRON | |
| TMR2_ROP_STARTS_TMRON_ERSHIGH | |
| TMR2_ROP_STARTS_TMRON_ERSLOW | |
| TMR2_ROP_RESETS_ERSBOTHEDGE | |
| TMR2_ROP_RESETS_ERSRISINGEDGE | |
| TMR2_ROP_RESETS_ERSFALLINGEDGE | |
| TMR2_ROP_RESETS_ERSLOW | |
| TMR2_ROP_RESETS_ERSHIGH | |
| TMR2_OS_STARTS_TMRON | |
| TMR2_OS_STARTS_ERSRISINGEDGE | |
| TMR2_OS_STARTS_ERSFALLINGEDGE | |
| TMR2_OS_STARTS_ERSBOTHEDGE | |
| TMR2_OS_STARTS_ERSFIRSTRISINGEDGE | |
| TMR2_OS_STARTS_ERSFIRSTFALLINGEDGE | |
| TMR2_OS_STARTS_ERSRISINGEDGEDETECT | |
| TMR2_OS_STARTS_ERSFALLINGEDGEDETECT | |
| TMR2_OS_STARTS_TMRON_ERSHIGH | |
| TMR2_OS_STARTS_TMRON_ERSLOW | |
| TMR2_MS_STARTS_TMRON_ERSRISINGEDGEDETECT | |
| TMR2_MS_STARTS_TMRON_ERSFALLINGEDGEDETECT | |
| TMR2_MS_STARTS_TMRON_ERSBOTHEDGE |
source/tmr2_deprecated.h File Reference
Macros
-
#define TMR2_Read TMR2_CounterGet
Defines the Custom Name for the TMR2_CounterGet API. The TMR2_Read will be deprecated in the future release. Use TMR2_CounterGet instead.
-
#define Timer2_Read TMR2_CounterGet
Defines the Custom Name for the TMR2_CounterGet API. The Timer2_Read will be deprecated in the future release. Use Timer2_CounterGet instead.
-
#define TMR2_Write TMR2_CounterSet
Defines the Custom Name for the TMR2_CounterSet API. The TMR2_Write will be deprecated in the future release. Use TMR2_CounterSet instead.
-
#define Timer2_Write TMR2_CounterSet
Defines the Custom Name for the TMR2_CounterSet API. The Timer2_Write will be deprecated in the future release. Use Timer2_CounterSet instead.
-
#define TMR2_PeriodCountSet TMR2_PeriodSet
Defines the Custom Name for the TMR2_PeriodSet API. The TMR2_PeriodCountSet will be deprecated in the future release. Use TMR2_PeriodSet instead.
-
#define Timer2_PeriodCountSet TMR2_PeriodSet
Defines the Custom Name for the TMR2_PeriodSet API. The Timer2_PeriodCountSet will be deprecated in the future release. Use Timer2_PeriodSet instead.
-
#define TMR2_OverflowCallbackRegister TMR2_PeriodMatchCallbackRegister
Defines the Custom Name for the TMR2_PeriodMatchCallbackRegister API. The TMR2_OverflowCallbackRegister will be deprecated in the future release. Use TMR2_PeriodMatchCallbackRegister instead.
-
#define Timer2_OverflowCallbackRegister TMR2_PeriodMatchCallbackRegister
Defines the Custom Name for the TMR2_PeriodMatchCallbackRegister API. The Timer2_OverflowCallbackRegister will be deprecated in the future release. Use Timer2_PeriodMatchCallbackRegister instead.
source/tmr2_drv.c File Reference
#include <xc.h> #include "../tmr2.h"
Functions
static void TMR2_DefaultPeriodMatchCallback (void)
void TMR2_Initialize (void)
Initializes the Timer2 (TMR2) module. This routine must be called before any other TMR2 routines.
void TMR2_Deinitialize (void)
Deinitializes the TMR2 to POR values.
void TMR2_Start (void)
Starts the TMR2 timer.
void TMR2_Stop (void)
Stops the TMR2 timer.
uint32_t TMR2_CounterGet (void)
Returns the current counter value.
void TMR2_CounterSet (uint32_t count)
Sets the counter value.
void TMR2_PeriodSet (uint32_t periodVal)
Sets the period count value.
uint32_t TMR2_PeriodGet (void)
Returns the current period count value.
uint32_t TMR2_MaxCountGet (void)
Returns the TMR2 maximum count value.
void TMR2_ISR (void)
Interrupt Service Routine (ISR) for the TMR2 period match interrupt.
void TMR2_PeriodMatchCallbackRegister (void(*callbackHandler)(void))
Setter function for the TMR2 period match event.
Variables
const struct TIMER_INTERFACE Timer2
static void(* TMR2_PeriodMatchCallback )(void)
Function Documentation
TMR2_DefaultPeriodMatchCallback()
static void TMR2_DefaultPeriodMatchCallback (void )[static]
Variable Documentation
Timer2
const struct TIMER_INTERFACE Timer2
Initial value:
= {
.Initialize = TMR2_Initialize,
.Deinitialize = TMR2_Deinitialize,
.Start = TMR2_Start,
.Stop = TMR2_Stop,
.PeriodSet = TMR2_PeriodSet,
.PeriodGet = TMR2_PeriodGet,
.CounterGet = TMR2_CounterGet,
.CounterSet = TMR2_CounterSet,
.MaxCountGet = TMR2_MaxCountGet,
.TimeoutCallbackRegister = TMR2_PeriodMatchCallbackRegister,
.Tasks = NULL
}
Section: Included Files
TMR2_PeriodMatchCallback
void(* TMR2_PeriodMatchCallback) (void)[static]
source/tmr2_drv.h File Reference
#include <stdint.h> #include <stdbool.h> #include "timer_interface.h"
Functions
void TMR2_Initialize (void)
Initializes the Timer2 (TMR2) module. This routine must be called before any other TMR2 routines.
void TMR2_Deinitialize (void)
Deinitializes the TMR2 module.
void TMR2_Start (void)
Starts the TMR2 timer.
void TMR2_Stop (void)
Stops the TMR2 timer.
uint32_t TMR2_CounterGet (void)
Returns the current counter value.
void TMR2_CounterSet (uint32_t count)
Sets the counter value.
void TMR2_PeriodSet (uint32_t periodVal)
Sets the period count value.
uint32_t TMR2_PeriodGet (void)
Returns the current period value.
uint32_t TMR2_MaxCountGet (void)
Returns the maximum count value of the timer.
void TMR2_ISR (void)
Interrupt Service Routine (ISR) for the TMR2 period match event.
void TMR2_Tasks (void)
Performs tasks to be executed during the TMR2 period match event.
void TMR2_PeriodMatchCallbackRegister (void(*callbackHandler)(void))
Registers a callback function for the TMR2 period match event.
Macros
#define TMR2_MAX_COUNT (255U)
Defines the TMR2 maximum count value.
#define TMR2_CLOCK_FREQ (250000UL)
Defines the TMR2 prescaled clock frequency in hertz.
-
#define TIMER2_MAX_COUNT TMR2_MAX_COUNT
Defines the Custom Name for the TMR2_MAX_COUNT.
-
#define TIMER2_CLOCK_FREQ TMR2_CLOCK_FREQ
Defines the Custom Name for the TMR2_CLOCK_FREQ.
-
#define Timer2_Initialize TMR2_Initialize
Defines the Custom Name for the TMR2_Initialize API.
-
#define Timer2_Deinitialize TMR2_Deinitialize
Defines the Custom Name for the TMR2_Deinitialize API.
-
#define Timer2_Start TMR2_Start
Defines the Custom Name for the TMR2_Start API.
-
#define Timer2_Stop TMR2_Stop
Defines the Custom Name for the TMR2_Stop API.
-
#define Timer2_CounterGet TMR2_CounterGet
Defines the Custom Name for the TMR2_CounterGet API.
-
#define Timer2_CounterSet TMR2_CounterSet
Defines the Custom Name for the TMR2_CounterSet API.
#define Timer2_PeriodSet TMR2_PeriodSet
Defines the Custom Name for the TMR2_PeriodSet API.
#define Timer2_PeriodGet TMR2_PeriodGet
Defines the Custom Name for the TMR2_PeriodGet API.
-
#define Timer2_MaxCountGet TMR2_MaxCountGet
Defines the Custom Name for the TMR2_MaxCountGet API.
-
#define Timer2_PeriodMatchCallbackRegister TMR2_PeriodMatchCallbackRegister
Defines the Custom Name for the TMR2_PeriodMatchCallbackRegister API.
-
#define Timer2_ISR TMR2_ISR
Defines the Custom Name for the TMR2_ISR API.
-
#define Timer2_Tasks TMR2_Tasks
Defines the Custom Name for the TMR2_Tasks API.
Variables
const struct TIMER_INTERFACE Timer2
Variable Documentation
Timer2
const struct TIMER_INTERFACE Timer2
Section: Included Files