7.2.1 Word Address Values
During an I2C write packet, the ATECC608A-TNGTLS interprets the second byte sent as the word address, which indicates the packet function as it is described in the table below:
| Name | Value | Description |
|---|---|---|
| Reset | 0x00 | Reset the address counter. The next I2C read or write transaction will start with the beginning of the I/O buffer. |
| Sleep (Low-power) | 0x01 | The ATECC608A-TNGTLS goes into the low-power Sleep mode and ignores all subsequent I/O transitions until the next Wake flag. The entire volatile state of the device is reset. |
| Idle | 0x02 | The ATECC608A-TNGTLS goes into the Idle mode and ignores all subsequent I/O transitions until the next Wake flag. The contents of TempKey, MessageDigestBuffer, and Alternate Key registers are retained. |
| Command | 0x03 | Write subsequent bytes to sequential addresses in the input command buffer that follow previous writes. This is the normal operation. |
| Reserved | 0x04 – 0xFF | These addresses should not be sent to the device. |