5.2.4.2 Verify - Stored Public Key Mode
When using the Verify command in Stored mode, the
public key to be used is stored in a data slot and does not need to be passed. Prior
to this command being run, the message should be written to TempKey or the Message
Digest Buffer using the Nonce command.
Procedure to Verify a Message with a Stored Key
- If so required, validate the
public key before using the
Verifycommand. - If so required, authorize the public key before use.
- Write the 32-byte digest of the
message to either the TempKey or Message Digest Buffer using the
Noncecommand in Fixed mode. - Write the System Nonce to either
the lower or upper 32 bytes of the Message Digest Buffer.
- If TempKey contains the message digest, then store the System Nonce in the lower 32 bytes of the Message Digest Buffer.
- If the message digest is
stored in the lower 32 bytes of the Message Digest Buffer, then store
the System Nonce in the upper 32 bytes of the Message Digest Buffer. The
user needs to write both the message digest and the System Nonce at one
time using the
Noncecommand.
- Issue the
Verifycommand. Include the Mode, KeyID, which specifies the public key slot, the 64-byte signature and the slot # of the internal public key. - The output will return:
- One byte success, fail or error code if MAC is not required.
- A 32-byte MAC, if specified by the mode or an error code, if the command fails.
|
Opcode |
Mode |
Public Key | Data Field (64 Bytes) | Comment |
|---|---|---|---|---|
|
Signature | ||||
| 0x45 | 0x00 | 0x00, 0[Slot] |
R value |
- Message stored in TempKey |
| 0x20 | 0x00, 0[Slot] |
R value |
- Message stored in Message Digest Buffer | |
| 0x80 | 0x00, 0[Slot] |
R value |
- Message stored in TempKey | |
| 0xA0 | 0x00, 0[Slot] |
R value |
- Message stored in Message Digest Buffer |
| Name | Mode | Size | Response |
|---|---|---|---|
| Response | 0x00 or 0x20 | 1 byte |
|
| 0x80 or 0xA0 |
32 bytes |
|
|
Size | Message in TempKey | Message in Message Digest Bufffer |
|---|---|---|
| 32 | Contents of the IO protection key | Contents of the IO protection key |
| 32 | Message from TempKey | First 32 bytes message from the Digest Buffer |
| 32 | System Nonce in the first 32 bytes of the Message Digest Buffer | System Nonce stored in the second 32 bytes of the Message Digest Buffer |
| 32 | R Data of the passed signature | R Data of the passed signature |
| 32 | S Data of the passed signature | S Data of the passed signature |
| 1 | Opcode | Opcode |
| 1 | Mode | Mode |
| 2 | Param2 [LSB,MSB] | Param2 [LSB,MSB] |