1.38.25.3 TRAM_DataScrambleKeySet Function
C
void TRAM_DataScrambleKeySet ( uint32_t dsckey )
Summary
Sets the key for data scrambling of the TrustRAM
Description
This function is used to set the key for data scrambling of the TrustRAM.
Precondition
Data scrambling has to be disabled using TRAM_DataScrambleEnable() function before calling this function to set the key.
Parameters
Param | Description |
---|---|
dsckey | Data Scramble Key. |
Returns
None.
Example
// Disable Data Scrambling TRAM_DataScrambleEnable(false); TRAM_DataScrambleKeySet(0x123456);
Remarks
None.