1.19.13 (PMP)

The Parallel Master Port (PMP) is a parallel 8-bit/16-bit I/O module specifically designed to communicate with a wide variety of parallel devices such as communications peripherals, LCDs, external memory devices and micro-controllers. Because the interfaces to parallel peripherals vary significantly, the PMP module is highly configurable.

Using The Library

The key features of PMP :-

  • 8-bit,16-bit interface

  • Up to 16 programmable address lines

  • Up to two Chip Select lines

  • Programmable strobe options

  • Address auto-increment/auto-decrement

  • Programmable address/data multiplexing

  • Programmable polarity on control signals

  • Programmable Wait states

Library Interface

peripheral library provides the following interfaces:

Functions

Name Description
PMP_Initialize This function initializes the PMP controller of the device
PMP_AddressSet Sets the current address of the PMP module to the specified address
PMP_AddressGet Gets the current address of the PMP module
PMP_MasterSend Sends the specified data in Master mode
PMP_MasterReceive Receives the data in Master mode
PMP_PortIsBusy Identifies if the (Master mode) PMP port is busy
PMP_AddressPortEnable Enables the port lines specified as PMP address lines
PMP_AddressPortDisable Disables the port lines specified as PMP address lines