1.20.6.9 DMAC_ChannelTransferStatusGet Function
C
DMAC_TRANSFER_EVENT DMAC_ChannelTransferStatusGet(DMAC_CHANNEL channel)
Summary
Returns the DMA channel's transfer status
Description
Returns the DMA channel's transfer status
Precondition
DMAC should have been initialized by calling the DMAC_Initialize.
Parameters
Param | Description |
---|---|
DMAC_CHANNEL channel | the particular channel to be interrogated |
Returns
- DMAC_TRANSFER_EVENT - enum of type DMAC_TRANSFER_EVENT indicating the status of the DMA transfer
Example
bool isBusy;
isBusy = DMAC_ChannelIsBusy(DMAC_CHANNEL_0);
if (isBusy == false)
{
if (DMAC_ChannelTransferStatusGet() == DMAC_TRANSFER_EVENT_ERROR)
{
// DMA transfer error
}
else
{
// DMA transfer successful
}
}
Remarks
None.