1.24.23.8 UARTx_WriteCallbackRegister Function
C
/* x = UART instance number */ /* Non-blocking mode */ void UARTx_WriteCallbackRegister( UART_CALLBACK callback, uintptr_t context ) /* Ring buffer mode */ void UARTx_WriteCallbackRegister( UART_RING_BUFFER_CALLBACK callback, uintptr_t context)
Summary
Sets the pointer to the function (and it's context) to be called when the given UART's write events occur.
Description
This function sets the pointer to a client function to be called "back" when the given UART's write events occur. It also passes a context value (usually a pointer to a context structure) that is passed into the function when it is called.
Precondition
UARTx_Initialize must have been called for the associated UART instance.
Parameters
Param | Description |
---|---|
callback | Pointer to the function to be called when the write transfer has completed. Setting this to NULL will disable the callback feature. |
context | A value (usually a pointer) passed (unused) into the function identified by the callback parameter. |
Returns
None.
Example
Non-blocking mode
void UARTWriteEventHandler ( uintptr_t context ) { if(UART1_ErrorGet() != UART_ERROR_NONE) { //Handle error case } else { //Transfer completed successfully } } UART1_WriteCallbackRegister(UARTWriteEventHandler, (uintptr_t)NULL);
Ring buffer mode
bool txThresholdEventReceived = false;
void UARTWriteEventHandler(UART_EVENT event, uintptr_t context )
{
if (event == UART_EVENT_WRITE_THRESHOLD_REACHED)
{
txThresholdEventReceived = true;
}
}
UART1_WriteCallbackRegister(UARTWriteEventHandler, (uintptr_t)NULL);
Remarks
None