1.37.2.3 ADCx_Disable Function
C
void ADCx_Disable( void ); // x is instance of the peripheral and it is applicable only for devices having multiple instances of the peripheral.
Summary
Disables given instance of ADC peripheral.
Description
This function disables the given instance of ADC.
Precondition
ADCx_Initialize() function must have been called first for the associated instance.
Parameters
None.
Returns
None.
Example
ADC0_Initialize();
ADC0_Enable();
//perform conversion
ADC0_Disable();
Remarks
If ADC instance is operating in slave mode, do not call ADCx_Disable function. Slave ADC is enabled/disabled by master ADC.