1.24.19.7 RTCC_CallbackRegister Function
C
void RTCC_CallbackRegister(RTC_CALLBACK callback, uintptr_t context);
Summary
Registers the function to be called from interrupt.
Description
This function registers the callback function to be called from interrupt.
Precondition
RTCC_Initialize must have been called.
Parameters
Param | Description |
---|---|
callback | Function of type RTC_CALLBACK. This will be called from the interrupt service routine for RTCC. |
context | Allows the caller to provide a context value (usually a pointer to the callers context for multi-instance clients). |
Returns
None.
Example
void RTC_Callback( uintptr_t context)
{
// Code to be executed in the RTCC callback
}
RTCC_CallbackRegister(RTC_Callback, (uintptr_t) NULL);
Remarks
The callback function will be executed in an interrupt context. Avoid calling blocking functions, performing computationally intensive operations or interrupt unsafe functions from the callback function.