1.18.19.7 TMRx_PeriodGet Function
C
/* x = TMR instance number */
uint16_t TMRx_PeriodGet(void);
Summary
Reads the period value of given timer.
Description
This function reads the value of period of a given timer.
Precondition
TMRx_Initialize() function must have been called first.
Parameters
None.
Returns
The timer's period value.
Example
uint16_t period; TMR2_Initialize(); period = TMR2_PeriodGet();
Remarks
If timer is operating on 32 bit mode then return value should be uint32_t type.