1.11.13.7 ICAPx_CaptureBufferRead Function
C
/* x = ICAP instance number */ uint32_t ICAPx_CaptureBufferRead (void)
Summary
This function will return the value contained in the ICAPx peripheral buffer. Based on the selected C32 capture, the return type will be uint16_t for 16 bit mode or uint32_t for 32 bit mode. Refer the generated header file for the actual function signature.
Description
This function will return the value contained in the ICAPx peripheral buffer.
Precondition
ICAPx_Initialize() function must have been called first.
Parameters
None.
Returns
uint32_t - Captured value from ICAPx peripheral buffer.
Example
uint32_t captureBuffer = 0;
ICAP1_Enable();
captureBuffer = ICAP1_CaptureBufferRead();
Remarks
Based on C32 capture select return type will be uint16_t for 16 bit mode.