1.38.20.41 RTC_Timer16Compare3HasMatched Function
C
bool RTC_Timer16Compare3HasMatched(void)
Summary
Returns true if the 16-bit Timer Compare 3 value has matched the counter.
Description
This function returns true if the 16-bit Timer Compare 3 value has matched the counter. When operating in 16-bit Timer Counter mode, the RTC peripheral compares the counter value with compare values (Compare 3). This function will return true if the counter value has matched the Compare 3 value. The Compare 3 Value could have been configured via MHC or at run time by calling the RTC_Timer16Compare3Set() function. The RTC_Timer16Compare3ValueMatched() function allows the application to poll for the compare value match.
Precondition
RTC_Initialize, RTC_Timer16Start must have been called for the associated RTC instance. The RTC value should have been configured for 16-bit Timer Counter Mode.
Parameters
None.
Returns
True, if Counter has matched Compare 3 Value and False otherwise.
Example
RTC_Initialize(); RTC_Timer16CounterSet(0); RTC_Timer16PeriodSet(0xFFF); // Calling the RTC_Timer16Compare3Set() function will override the RTC_Timer16Compare3Set(0x3F); RTC_Timer16Start(); // Wait till the Compare 3 value has matched. while(!RTC_Timer16Compare3HasMatched());
Remarks
This API is available for devices that have more than three compare register in 16-bit mode.