1.15.12.4 NVM_DoubleWordWrite Function
C
bool NVM_DoubleWordWrite( uint32_t *data, const uint32_t address );
Summary
Writes two words into the Flash.
Description
Writes two words (8 bytes) at the given address.
Precondition
None
Parameters
Param | Description |
---|---|
data | Pointer to the buffer which holds data to be written. |
address | Address at which the data will be written. |
Returns
Always return true.
Example
NVM_DoubleWordWrite(data_to_fill, 0x9D100000);