1.4.2.7 ADCx_ConversionResultGet Function
C
uint16_t ADCx_ConversionResultGet( void ); // x is instance of the peripheral and it is applicable only for devices having multiple instances of the peripheral.
Summary
Returns the conversion result of the channel.
Description
This function returns the result of completed conversion of the channel.
Precondition
ADCx_Initialize() function must have been called first for the associated instance.And conversion must have been started. Also check whether result is ready to read.
Parameters
None.
Returns
adcResult - conversion result of the channel.
Example
uint16_t adcResult = 0;
ADC0_Initialize();
ADC0_ConversionStart();
while(!ADC0_ConversionStatusGet());
adcResult = ADC0_ConversionResultGet();
Remarks
This function can be called from interrupt or by polling the status when result is available. User should decode the result based on result sign mode (differential mode) and result resolution (8, 10, 12 or 16 bit) configuration.