1.13.7.7 DMAC_ChannelDisable Function

C

void DMAC_ChannelDisable(DMAC_CHANNEL channel)

Summary

This function disables the DMA channel.

Description

The function disables the specified DMAC channel. Once disabled, the channel will ignore triggers and will not transfer data till the next time a DMAC_ChannelTransfer function is called. If there is a transfer already in progress, this will aborted. If there were multiple linked transfers assigned on the channel, the on-going transfer will be aborted and the other descriptors will be discarded.

Precondition

DMAC should have been initialized by calling DMAC_Initialize.

Parameters

Param Description
DMAC_CHANNEL channel the particular channel to be disabled

Returns

None.

Example

DMAC_ChannelDisable (DMAC_CHANNEL_0);