1.6.17.7 PAC_CALLBACK Typedef
C
typedef void (*PAC_CALLBACK)( uintptr_t context );
Summary
Defines the data type and function signature for the PAC peripheral callback function.
Description
This data type defines the function signature for the PAC peripheral callback function. The PAC peripheral will call back the function with this signature when a access violation has been detected.
Precondition
None.
Parameters
Param | Description |
---|---|
context | Allows the caller to provide a context value (usually a pointer to the callers context for multi-instance clients). |
Returns
None.
Example
void APP_PACErrorCallback( uintptr_t context )
{
// PAC Error occurred. Fix the root-cause so that PAC error never occurs.
}
PAC_CallbackRegister(APP_PACErrorCallback, NULL);
Remarks
The callback feature is only available when the library was generated with interrupt option (in MHC) enabled.
The function will execute within an interrupt context. Avoid calling computationally intensive or blocking functions from within the callback function.