1.6.21.19 RTC_Timer32Stop Function

C

void RTC_Timer32Stop ( void )

Summary

Stops the 32-bit timer from counting.

Description

This function will stop the 32-bit timer from counting. Any on-going timing/counting operations will be affected. Stopping the timer does not reset the counter. This must be explicitly done by calling the RTC_Timer32CounterSet() function.

Calling this function if the timer is already stopped will result in a functional no-operation. An application may need to stop the timer if it does not require delay services or if the counting needs to paused.

Precondition

RTC_Initialize must have been called for the associated RTC instance. The RTC peripheral should have been configured in 32-bit Timer Counter mode.

Parameters

None.

Returns

None.

Example

// Refer to the description of the RTC_Timer32CounterHasOverflowed()
// function for example usage of the RTC_Timer32Stop() function.

Remarks

None.