1.16.13.5 PMP_MasterReceive Function
C
uint32_t PMP_MasterReceive( void )
Summary
Receives the data in Master mode.
Description
This function receives the data. The flow of data is from the slave to the master.
Precondition
PMP should have been initialized by calling PMP_Initialize and configured for Master mode.
Parameters
None.
Returns
uint32_t - Data received
Example
uint32_t data;
PMP_Initialize();
PMP_AddressSet(0x1);
if(!PMP_PortIsBusy())
{
data = PMP_MasterReceive();
}
Remarks
None.