1.40.20.61 SERCOMx_I2C_TransferSetup Function

C

/* x = SERCOM instance number */

/* I2C master mode */

bool SERCOMx_I2C_TransferSetup(SERCOM_I2C_TRANSFER_SETUP* setup, uint32_t srcClkFreq)	

Summary

Dynamic setup of SERCOM I2C Peripheral

Description

This API is generally used when there are multiple clients on the same I2C bus having different I2C clock speed. In such a case, the SERCOMx_I2C_TransferSetup API must be called to set the appropriate I2C bus speed before starting the I2C transfer for the I2C slave.

Precondition

SERCOMx_I2C_Initialize must have been called for the associated SERCOM I2C instance. The transfer status should not be busy.

Parameters

Param Description
setup Pointer to the structure containing the transfer setup
srcClkFreq SERCOM I2C Peripheral Clock Source Frequency

Returns

true - Transfer setup was updated Successfully.

false - Failure while updating transfer setup.

Example

SERCOM_I2C_TRANSFER_SETUP setup;

setup.clkSpeed = 400000;

// Make sure that the I2C is not busy before changing the I2C clock frequency
if (SERCOM0_I2C_I2C_IsBusy() == false)
{
    if (SERCOM0_I2C_TransferSetup( &setup, 0 ) == true)
    {
        // Transfer Setup updated successfully
    }
}

Remarks

srcClkFreq overrides any change in the peripheral clock frequency. If configured to zero PLIB takes the peripheral clock frequency from MHC.