1.3.25.46 SERCOMx_SPI_Initialize Function
C
/* x = SERCOM instance number */ /* SPI master and slave mode */ void SERCOMx_SPI_Initialize (void);
Summary
Initializes instance x of the SERCOM module in SPI master or slave mode.
Description
This function initializes instance x of SERCOM module in SPI master or slave mode. This function should be called before any other library function. The SERCOM module will be configured as per the MHC settings.
Precondition
MCC GUI should be configured with the right values
Parameters
None.
Returns
None.
Example
SERCOM0_SPI_Initialize();
Remarks
This function must be called once before any other SPI function is called