1.24.8.4 DMT_CounterGet Function
C
uint32_t DMT_CounterGet( void )
Summary
Returns the DMT current counter value.
Description
This function returns the current DMT counter value. The value is the number of instructions counted since the count was last cleared.
Precondition
DMT must be enabled using DMT_Enable().
Parameters
None.
Returns
The current counter value.
Example
uint32_t value = 0;
DMT_Enable();
value = DMT_CounterGet();
Remarks
None.