1.2.17.19 PORT_PinGPIOConfig Function

C

void PORT_PinGPIOConfig(PORT_PIN pin)

Summary

Configures the selected pin as GPIO

Description

This function configures the given port pin as GPIO.

Precondition

The PORT_Initialize() function should have been called.

Parameters

Param Description
pin One of the IO port pin from the enum PORT_PIN

Returns

None.

Example

// Enable port pin PB01 as GPIO
PORT_PinGPIOConfig(PORT_PIN_PB01);

Remarks

None.