1.22.17.6 OCMPx_CompareValueGet Function
C
/* x = OCMP instance number */ uint32_t OCMPx_CompareValueGet (void)
Summary
Reads the compare value. Based on OC32 bit, compare value will be 16-bit or 32-bit. Refer the generated header file for the exact function signature.
Description
This function reads the value of the compare register
Precondition
OCMPx_Initialize() function must have been called first.
Parameters
void
Returns
uint32_t - Compare register value
Example
uint32_t compare; OCMP1_Initialize(); OCMP1_Enable(); compare = OCMP1_CompareValueGet();
Remarks
Based on OC32 bit, compare value will be 16-bit or 32-bit. Refer the generated header file for the exact function signature.